Macros | |
| #define | DebugP_ASSERT_ENABLED 1 |
| #define | DebugP_LOG_ENABLED 1 |
| #define | DEBUGP_LOGFXN_REGISTER_SUCCESS (0) |
| DebugP Log Function registration return types. More... | |
| #define | DEBUGP_LOGFXN_ALREADY_REGISTERD (-1) |
| #define | DebugP_assert(expression) |
Typedefs | |
| typedef void(* | DebugP_exptnLogFxn) (const char *format,...) |
| Assert Enabled. More... | |
Functions | |
| void | Osal_DebugP_assert_fcn (bool expression, const char *filename, int32_t line) |
| Assert checking function. More... | |
| void | DebugP_exceptionLog (const char *format, uint32_t arg1, uint32_t arg2) |
| DebugP Exception state log function. It takes a pair of values to be printed during exception dump. More... | |
| void | DebugP_log0 (const char *format) |
| Debug log function with 0 parameters. More... | |
| int32_t | DebugP_registerExcptnLogFxn (DebugP_exptnLogFxn fxn) |
| Debug log function registration. More... | |
| void | DebugP_deRegisterExcptnLogFxn (void) |
| Debug log function deregistration. More... | |
| void | DebugP_log1 (const char *format, uintptr_t p1) |
| Debug log function with 1 parameters. More... | |
| void | DebugP_log2 (const char *format, uintptr_t p1, uintptr_t p2) |
| Debug log function with 2 parameters. More... | |
| void | DebugP_log3 (const char *format, uintptr_t p1, uintptr_t p2, uintptr_t p3) |
| Debug log function with 3 parameters. More... | |
| void | DebugP_log4 (const char *format, uintptr_t p1, uintptr_t p2, uintptr_t p3, uintptr_t p4) |
| Debug log function with 4 parameters. More... | |
DebugP interface
| #define DebugP_ASSERT_ENABLED 1 |
| #define DebugP_LOG_ENABLED 1 |
| #define DEBUGP_LOGFXN_REGISTER_SUCCESS (0) |
DebugP Log Function registration return types.
DEBUGP_PRINTFXN_REGISTER_SUCCESS is returned on succesful registration of log API. DEBUGP_PRINTFXN_ALREADY_REGISTERD is returned, if an API is already registered.
| #define DEBUGP_LOGFXN_ALREADY_REGISTERD (-1) |
| #define DebugP_assert | ( | expression | ) |
| typedef void(* DebugP_exptnLogFxn) (const char *format,...) |
Assert Enabled.
The defintion is used to control the feature if assertions are to be enabled or not. This flag can be enabled for debug builds by changing the file OR through the makefile.
Log Enabled
The defintion is used to plug the logging API to the OS provided logging mechansim Application developers can port the backend Logging API as per their requirements
DebugP Log Function signature to be used for printing
| void Osal_DebugP_assert_fcn | ( | bool | expression, |
| const char * | filename, | ||
| int32_t | line | ||
| ) |
Assert checking function.
If the expression is evaluated to true, the API does nothing. If it is evaluated to false, the underlying RTOS port implementation handles the assert via its mechanisms.
| expression | Expression to evaluate |
| filename | File name |
| line | Line number where evaluation occurs |
| void DebugP_exceptionLog | ( | const char * | format, |
| uint32_t | arg1, | ||
| uint32_t | arg2 | ||
| ) |
DebugP Exception state log function. It takes a pair of values to be printed during exception dump.
| format | "printf" format string |
| arg1 | first parameter to format string |
| arg2 | second parameter to format string |
| void DebugP_log0 | ( | const char * | format | ) |
Debug log function with 0 parameters.
The underlying RTOS port implementation handles the logging via its mechanisms.
| format | "printf" format string |
| int32_t DebugP_registerExcptnLogFxn | ( | DebugP_exptnLogFxn | fxn | ) |
Debug log function registration.
Application needs to call this API to register its print API.
| fxn | Function pointer for print function to be registerd. |
| void DebugP_deRegisterExcptnLogFxn | ( | void | ) |
Debug log function deregistration.
Application needs to call this API to de-register its print API.
| void DebugP_log1 | ( | const char * | format, |
| uintptr_t | p1 | ||
| ) |
Debug log function with 1 parameters.
The underlying RTOS port implementation handles the logging via its mechanisms.
| format | "printf" format string |
| p1 | first parameter to format string |
| void DebugP_log2 | ( | const char * | format, |
| uintptr_t | p1, | ||
| uintptr_t | p2 | ||
| ) |
Debug log function with 2 parameters.
The underlying RTOS port implementation handles the logging via its mechanisms.
| format | "printf" format string |
| p1 | first parameter to format string |
| p2 | second parameter to format string |
| void DebugP_log3 | ( | const char * | format, |
| uintptr_t | p1, | ||
| uintptr_t | p2, | ||
| uintptr_t | p3 | ||
| ) |
Debug log function with 3 parameters.
The underlying RTOS port implementation handles the logging via its mechanisms.
| format | "printf" format string |
| p1 | first parameter to format string |
| p2 | second parameter to format string |
| p3 | third parameter to format string |
| void DebugP_log4 | ( | const char * | format, |
| uintptr_t | p1, | ||
| uintptr_t | p2, | ||
| uintptr_t | p3, | ||
| uintptr_t | p4 | ||
| ) |
Debug log function with 4 parameters.
The underlying RTOS port implementation handles the logging via its mechanisms.
| format | "printf" format string |
| p1 | first parameter to format string |
| p2 | second parameter to format string |
| p3 | third parameter to format string |
| p4 | fourth parameter to format string |