PSDK QNX API Guide
RegisterIntr.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-present, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
48 #ifndef ti_osal_RegisterIntr__include
49 #define ti_osal_RegisterIntr__include
50 
51 #include <ti/osal/EventCombinerP.h>
52 #include <ti/osal/HwiP.h>
53 #include <ti/osal/MuxIntcP.h>
54 
55 #ifdef __cplusplus
56 extern "C" {
57 #endif
58 
59 #include <stdint.h>
60 #include <stdbool.h>
61 #include <stddef.h>
62 typedef void (*Osal_IsrRoutine)(uintptr_t arg);
66 typedef struct {
67  char *name;
68  uint32_t corepacEventNum;
69  uint32_t intVecNum;
71  uintptr_t arg;
72  uint32_t priority;
84  uint32_t triggerSensitivity;
92  uint32_t enableIntr;
95 #ifdef QNX_OS
96  uint32_t intAutoEnable;
97 #endif
99 
103 #define OSAL_REGINT_INTVEC_EVENT_COMBINER (16U)
104 
108 typedef struct {
109  MuxIntcP_inParams *muxInParams;
110  MuxIntcP_outParams *muxOutParams;
112 
120 typedef struct {
126 
135 typedef int32_t OsalInterruptRetCode_e;
137 #define OSAL_INT_SUCCESS ((int32_t) 0)
139 #define OSAL_INT_ERR_INVALID_PARAMS ((int32_t) -1)
141 #define OSAL_INT_ERR_HWICREATE ((int32_t) -2)
143 #define OSAL_INT_ERR_EVENTCOMBINER_REG ((int32_t) -3)
145 #define OSAL_INT_ERR_DELETE ((int32_t) -4)
147 #define OSAL_INT_UNSUPPORTED ((int32_t) -5)
148 /* @} */
149 
160  HwiP_DirectFxn isrFxn, HwiP_Handle *hwiPHandlePtr);
170 OsalInterruptRetCode_e Osal_DeleteInterrupt(HwiP_Handle hwiPhandle,uint32_t corepacEventNum);
175 void Osal_EnableInterrupt(uint32_t corepacEvent,uint32_t interruptNum);
180 void Osal_DisableInterrupt(uint32_t corepacEvent,uint32_t interruptNum);
185 void Osal_ClearInterrupt(uint32_t corepacEvent,uint32_t interruptNum);
186 #ifdef __cplusplus
187 }
188 #endif
189 
190 #endif /* ti_osal_RegisterIntr__include */
191 /* @} */
Hardware Interrupt module for the RTOS Porting Interface.
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:81
void(* HwiP_DirectFxn)(void)
Prototype for the entry function for a hardware interrupt registered using HwiP_createDirect.
Definition: HwiP.h:127
OsalRegisterIntParams_corepac_t corepacConfig
Definition: RegisterIntr.h:121
void(* Osal_IsrRoutine)(uintptr_t arg)
Definition: RegisterIntr.h:62
char * name
Definition: RegisterIntr.h:67
uintptr_t arg
Definition: RegisterIntr.h:71
void Osal_EnableInterrupt(uint32_t corepacEvent, uint32_t interruptNum)
Function to enable the interrupt corresponding to an event number.
uint32_t corepacEventNum
Definition: RegisterIntr.h:68
Osal_IsrRoutine isrRoutine
Definition: RegisterIntr.h:70
int32_t OsalInterruptRetCode_e
Return error codes for Osal Interrupt functions.
Definition: RegisterIntr.h:135
MuxIntcP_inParams * muxInParams
Definition: RegisterIntr.h:109
uint32_t priority
Definition: RegisterIntr.h:72
OsalInterruptRetCode_e Osal_RegisterInterruptDirect(OsalRegisterIntrParams_t *interruptRegParams, HwiP_DirectFxn isrFxn, HwiP_Handle *hwiPHandlePtr)
Function to register direct interrupt with parameters provided.
OsalRegisterIntParams_socmux_t socMuxConfig
Definition: RegisterIntr.h:122
void Osal_ClearInterrupt(uint32_t corepacEvent, uint32_t interruptNum)
Function to clear the interrupt corresponding to an event number.
OsalInterruptRetCode_e Osal_DeleteInterrupt(HwiP_Handle hwiPhandle, uint32_t corepacEventNum)
Function to delete interrupt corresponding to an event number.
MuxIntcP_outParams * muxOutParams
Definition: RegisterIntr.h:110
void Osal_RegisterInterrupt_initParams(OsalRegisterIntrParams_t *interruptRegParams)
Function to initialize the interrupt registration configuration data structure.
uint32_t enableIntr
Definition: RegisterIntr.h:92
void Osal_DisableInterrupt(uint32_t corepacEvent, uint32_t interruptNum)
Function to disable the interrupt corresponding to an event number.
uint32_t intVecNum
Definition: RegisterIntr.h:69
uint32_t triggerSensitivity
Definition: RegisterIntr.h:84
OsalInterruptRetCode_e Osal_RegisterInterrupt(OsalRegisterIntrParams_t *interruptRegParams, HwiP_Handle *hwiPHandlePtr)
Function to register interrupt with parameters provided.
Interrupt Configuration parameters for the corepac (c6x/a15/m5/a8/a9)
Definition: RegisterIntr.h:66
Interrupt Configuration parameters for soc mux prior to reaching the core.
Definition: RegisterIntr.h:108
Interrupt Configuration parameters This is the data structure used to configure the interrupts in the...
Definition: RegisterIntr.h:120