|
| file | udma_types.h |
| | UDMA Low Level Driver API/interface data types file.
|
| |
|
Error codes returned by UDMA APIs
|
| #define | UDMA_SOK (CSL_PASS) |
| | API call successful. More...
|
| |
| #define | UDMA_EFAIL (CSL_EFAIL) |
| | API call returned with error as failed. Used for generic error. It may be some hardware failure and/or software failure. More...
|
| |
| #define | UDMA_EBADARGS (CSL_EBADARGS) |
| | API call returned with error as bad arguments. Typically, NULL pointer passed to the API where its not expected. More...
|
| |
| #define | UDMA_EINVALID_PARAMS (CSL_EINVALID_PARAMS) |
| | API call returned with error as invalid parameters. Typically when parameters passed are not valid or out of range. More...
|
| |
| #define | UDMA_ETIMEOUT (CSL_ETIMEOUT) |
| | API call returned with error as timed out. Typically API is waiting for some condition and returned as condition not happened in the timeout period. More...
|
| |
| #define | UDMA_EALLOC (CSL_EALLOC) |
| | API call returned with error as allocation failed. More...
|
| |
|
This represents the various Instances in an SOC. The actual Instances present in the chip is SOC dependent. Refer soc file for the actual instance present. Kindly use Udma_InstanceIdSoc macros for SOC specific name.
|
| #define | UDMA_INST_ID_0 (0U) |
| |
| #define | UDMA_INST_ID_1 (1U) |
| |
| #define | UDMA_INST_ID_2 (2U) |
| |
| #define | UDMA_INST_ID_3 (3U) |
| |
This is UDMA driver common parameters and API
◆ UDMA_CACHELINE_ALIGNMENT
| #define UDMA_CACHELINE_ALIGNMENT (128U) |
Cache line size for alignment of descriptor and buffers.
◆ UDMA_SOK
| #define UDMA_SOK (CSL_PASS) |
◆ UDMA_EFAIL
| #define UDMA_EFAIL (CSL_EFAIL) |
API call returned with error as failed. Used for generic error. It may be some hardware failure and/or software failure.
◆ UDMA_EBADARGS
| #define UDMA_EBADARGS (CSL_EBADARGS) |
API call returned with error as bad arguments. Typically, NULL pointer passed to the API where its not expected.
◆ UDMA_EINVALID_PARAMS
| #define UDMA_EINVALID_PARAMS (CSL_EINVALID_PARAMS) |
API call returned with error as invalid parameters. Typically when parameters passed are not valid or out of range.
◆ UDMA_ETIMEOUT
| #define UDMA_ETIMEOUT (CSL_ETIMEOUT) |
API call returned with error as timed out. Typically API is waiting for some condition and returned as condition not happened in the timeout period.
◆ UDMA_EALLOC
| #define UDMA_EALLOC (CSL_EALLOC) |
API call returned with error as allocation failed.
◆ UDMA_NO_WAIT
| #define UDMA_NO_WAIT ((uint32_t) 0U) |
UDMA transaction timeout define - no wait.
◆ UDMA_WAIT_FOREVER
| #define UDMA_WAIT_FOREVER (~((uint32_t) 0U)) |
UDMA transaction timeout define - wait for ever.
◆ UDMA_INIT_DONE
| #define UDMA_INIT_DONE (0xABDCABCDU) |
Macro used to specify that init is performed for an object.
◆ UDMA_DEINIT_DONE
| #define UDMA_DEINIT_DONE (0x00000000U) |
Macro used to specify that deinit is performed for an object.
◆ UDMA_INST_ID_0
| #define UDMA_INST_ID_0 (0U) |
◆ UDMA_INST_ID_1
| #define UDMA_INST_ID_1 (1U) |
◆ UDMA_INST_ID_2
| #define UDMA_INST_ID_2 (2U) |
◆ UDMA_INST_ID_3
| #define UDMA_INST_ID_3 (3U) |
◆ UDMA_UTC_ID0
| #define UDMA_UTC_ID0 (0U) |
◆ UDMA_UTC_ID1
| #define UDMA_UTC_ID1 (1U) |
◆ UDMA_UTC_ID2
| #define UDMA_UTC_ID2 (2U) |
◆ UDMA_UTC_ID3
| #define UDMA_UTC_ID3 (3U) |
◆ UDMA_UTC_ID4
| #define UDMA_UTC_ID4 (4U) |
◆ UDMA_UTC_ID5
| #define UDMA_UTC_ID5 (5U) |
◆ UDMA_UTC_ID6
| #define UDMA_UTC_ID6 (6U) |
◆ UDMA_UTC_ID7
| #define UDMA_UTC_ID7 (7U) |
◆ UDMA_UTC_ID8
| #define UDMA_UTC_ID8 (8U) |
◆ UDMA_UTC_ID9
| #define UDMA_UTC_ID9 (9U) |
◆ UDMA_MAPPED_GROUP0
| #define UDMA_MAPPED_GROUP0 (0U) |
◆ UDMA_MAPPED_GROUP1
| #define UDMA_MAPPED_GROUP1 (1U) |
◆ UDMA_MAPPED_GROUP2
| #define UDMA_MAPPED_GROUP2 (2U) |
◆ UDMA_MAPPED_GROUP3
| #define UDMA_MAPPED_GROUP3 (3U) |
◆ UDMA_MAPPED_GROUP4
| #define UDMA_MAPPED_GROUP4 (4U) |
◆ UDMA_MAPPED_GROUP5
| #define UDMA_MAPPED_GROUP5 (5U) |
◆ UDMA_MAPPED_GROUP6
| #define UDMA_MAPPED_GROUP6 (6U) |
◆ UDMA_MAPPED_GROUP7
| #define UDMA_MAPPED_GROUP7 (7U) |