3.1. Release notes - 07_00_00¶
3.1.1. Documentation¶
The documentation included with the PSDKQA is specific to the PSDKQA package.
PSDKRA package documentation (PSDKRA Components) must also be referenced, for full understanding of PSDKQA support.
3.1.2. PSDKQA Features¶
Note
Reference PSDKRA package documentation (LINK) for an extensive list of new and current features supported by PSDKQA + PSDKRA. This section lists only the features that are PSDKQA specific.
Note
For features & drivers enabled by the QNX BSP, please refer to BSP Documentation or contact QNX.
3.1.2.1. Enabled in this Release¶
Features enabled in this release, specific to PSDKQA addon package are:
- A72 driver for CPSW9G
- UDMA Resource Manager
- IPC Resource Manager
- Vision Apps Encode Application
- SBL Boot flow support for QNX
3.1.2.2. Enabled in Previous Releases¶
Features enabled in previous release, specific to PSDKQA addon package are:
- A72 driver for CPSW2G + gPTP
- Shared Memory Allocator Resource Manager
- SCIClient Resource Manager
- A72 OpenVx Integraion
- A72 Vision Apps Demo Support
3.1.3. Software Dependencies¶
3.1.3.1. QNX Dependency¶
Note
The PSDKQA addon package is dependent on installations from QNX Software Center. The below QNX packages were used for PSDKQA_07_00_00 build and verfication.
| QNX Package | Build Identifier | Date |
|---|---|---|
| QNX SDP7.0 BSP for Texas Instruments Jacinto 7 J721E (DRA829/TDA4xM) Evaluation Modules | EXPERIMENTAL (7.0 BuildlD 29) | May 08, 2020 |
| QNX SDP 7.0 Graphics Implementation | STABLE (7.0 BuildlD 6529) | August 08, 2019 |
| QNX SDP7.0 Networking Middleware - Network manager, Wi-Fi manager, Tether manager | STABLE (7.0 BuildID 214) | July 19, 2018 |
| QNX SDP 7.0 Screen Board Supoort Jacinto 7 | EXPERIMENTAL (7.0 buildID 8001) | May 20, 2020 |
| QNX SDP 7.0 Screen Board Support Dummy | EXPERIMENTAL (7.0 BuildID 8001) | May 20, 2020 |
| QNX Software Development Platform 7.0 | STABLE (7.0.0 GA 201702151847) | Feb. 27, 2017 |
3.1.3.2. PSDKRA Dependency¶
The PSDKQA package is an addon package to the PSDKRA release, as such the PSDKRA is required.
3.1.3.3. PSDKLA Dependency¶
If SPL boot mode is to be supported, downloading the PSDKLA 07_00_00 package is recommended for access to the prebuilt binaries.
3.1.4. Device Support and Validation Information¶
| SoC | Build Host (OS) | Run Target (OS) | Test Plaform |
|---|---|---|---|
| J721e | x86_64 (Linux Ubuntu 18.04) | R5F, C6x, C7x running TI-RTOS A72 running QNX |
J721e EVM with daughter cards |
| PC emulation mode | x86_64 (Linux Ubuntu 18.04) | x86_64 (Linux Ubuntu 18.04) | x86_64 (Linux Ubuntu 18.04) |
3.1.5. Known Issues¶
A list of key known issues with the PSDKQA release is provided below.
Note
Refer to individual PSDKRA Components release notes for known issues in each component
| Index | Module | Description |
|---|---|---|
| 1 | SCI | The SCI Resource Manager will incorrectly generate a warning log that an ACK flag is not present. |
| 2 | devnp-cpsw2g | The devnp-cpsw2g driver must have its core affinity set, such that the driver only runs on the first instance of the A72. This avoids a resource conflict that is under investigation. |
| 3 | devnp-cpsw2g devnp-cpsw9g | In high traffic scenarios the transmit side may generate a log CPSW_UTILS_GET_PKT_DRIVER_STATE(pStateVar) == expectedState. This occurence of the log may coincide with a failure scenario. This issue is under investigation. |
| 4 | A72 DSS on HDMI | The A72 control of DSS on HDMI Display is not working in some senario. |
3.1.6. Additional Reports¶
For additional reports like test report, traceability refer PSDKRA Additional Reports