PSDK QNX API Guide

VDEV structure. Must match with Linux. More...

#include <ipc_rsctypes.h>

Data Fields

uint32_t type
 
uint32_t id
 
uint32_t notifyid
 
uint32_t dfeatures
 
uint32_t gfeatures
 
uint32_t config_len
 
uint8_t status
 
uint8_t num_of_vrings
 
uint8_t reserved [2]
 
uint32_t padding
 

Detailed Description

VDEV structure. Must match with Linux.


The documentation for this struct was generated from the following file: