UDMA Driver API/interface file. More...
#include <stdint.h>#include <ti/drv/udma/soc/udma_soc.h>#include <ti/csl/soc.h>#include <ti/csl/csl_psilcfg.h>#include <ti/csl/csl_intaggr.h>#include <ti/csl/csl_intr_router.h>#include <ti/osal/osal.h>#include <ti/drv/sciclient/sciclient.h>#include <ti/drv/udma/include/udma_cfg.h>#include <ti/drv/udma/include/udma_types.h>#include <ti/drv/udma/include/udma_osal.h>#include <ti/drv/udma/include/udma_ring.h>#include <ti/drv/udma/include/udma_proxy.h>#include <ti/drv/udma/include/udma_flow.h>#include <ti/drv/udma/include/udma_event.h>#include <ti/drv/udma/include/udma_rm.h>#include <ti/drv/udma/include/udma_ch.h>#include <ti/drv/udma/include/udma_utils.h>#include <unistd.h>Go to the source code of this file.
Data Structures | |
| struct | Udma_InitPrms |
| UDMA initialization parameters. More... | |
| struct | Udma_DrvHandle |
| UDMA driver object. More... | |
Macros | |
| #define | QNX_OS |
| #define | BUILD_MPU1_0 |
Typedefs | |
| typedef uint64_t(* | Udma_VirtToPhyFxn) (const void *virtAddr, uint32_t chNum, void *appData) |
| UDMA Virtual to Physical address translation callback function. More... | |
| typedef void *(* | Udma_PhyToVirtFxn) (uint64_t phyAddr, uint32_t chNum, void *appData) |
| UDMA Physical to Virtual address translation callback function. More... | |
| typedef void(* | Udma_PrintFxn) (const char *str) |
| UDMA info/debug print function prototype. More... | |
UDMA Ring Local API's function prototypes | |
|
Function prototypes for various local UDMA Ring API's. For Normal RA / LCDMA RA, function pointers will be used to call the appropriate function. | |
| typedef void(* | Udma_ringHandleClearRegsFxn) (Udma_RingHandle ringHandle) |
| UDMA Ring handle clear register function prototype. More... | |
| typedef void(* | Udma_ringSetDoorBellFxn) (Udma_RingHandle ringHandle, int32_t count) |
| UDMA Ring set doorbell function prototype. More... | |
| typedef void(* | Udma_ringPrimeFxn) (Udma_RingHandle ringHandle, uint64_t phyDescMem) |
| UDMA Ring prime function prototype. More... | |
| typedef void(* | Udma_ringPrimeReadFxn) (Udma_RingHandle ringHandle, uint64_t *phyDescMem) |
| UDMA Ring prime read function prototype. More... | |
| typedef void *(* | Udma_ringGetMemPtrFxn) (Udma_RingHandle ringHandle) |
| UDMA Ring get mem pointer function prototype. More... | |
| typedef uint32_t(* | Udma_ringGetModeFxn) (Udma_RingHandle ringHandle) |
| UDMA Ring get ring mode function prototype. More... | |
| typedef uint32_t(* | Udma_ringGetElementCntFxn) (Udma_RingHandle ringHandle) |
| UDMA Ring get element count function prototype. More... | |
| typedef uint32_t(* | Udma_ringGetForwardRingOccFxn) (Udma_RingHandle ringHandle) |
| UDMA Ring get forward ring occupancy function prototype. More... | |
| typedef uint32_t(* | Udma_ringGetReverseRingOccFxn) (Udma_RingHandle ringHandle) |
| UDMA Ring get reverse ring occupancy function prototype. More... | |
| typedef uint32_t(* | Udma_ringGetWrIdxFxn) (Udma_RingHandle ringHandle) |
| UDMA Ring get write index value function prototype. More... | |
| typedef uint32_t(* | Udma_ringGetRdIdxFxn) (Udma_RingHandle ringHandle) |
| UDMA Ring get read index value function prototype. More... | |
| typedef int32_t(* | Udma_ringDequeueRawFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t *phyDescMem) |
| UDMA Ring dequeue raw function prototype. More... | |
| typedef int32_t(* | Udma_ringQueueRawFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t phyDescMem) |
| UDMA Ring queue raw function prototype. More... | |
| typedef int32_t(* | Udma_ringFlushRawFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, uint64_t *phyDescMem) |
| UDMA Ring flush raw function prototype. More... | |
| typedef void(* | Udma_ringSetCfgFxn) (Udma_DrvHandle drvHandle, Udma_RingHandle ringHandle, const Udma_RingPrms *ringPrms) |
| UDMA Ring set Cfg function prototype. More... | |
| int32_t | Udma_init (Udma_DrvHandle drvHandle, const Udma_InitPrms *initPrms) |
| UDMA init function. More... | |
| int32_t | Udma_deinit (Udma_DrvHandle drvHandle) |
| UDMA deinit function. More... | |
| int32_t | UdmaInitPrms_init (uint32_t instId, Udma_InitPrms *initPrms) |
| Udma_InitPrms structure init function. More... | |
| static uint64_t | Udma_defaultVirtToPhyFxn (const void *virtAddr, uint32_t chNum, void *appData) |
| Default virtual to physical translation function. More... | |
| static void * | Udma_defaultPhyToVirtFxn (uint64_t phyAddr, uint32_t chNum, void *appData) |
| Default physical to virtual translation function. More... | |
UDMA Driver API/interface file.
Requirement: DOX_REQ_TAG(PDK-2494)