UDMA RM related parameters and API. More...
Go to the source code of this file.
Data Structures | |
| struct | Udma_RmInitPrms |
| UDMA resource manager init parameters. More... | |
| struct | Udma_RmSharedResPrms |
| UDMA resource manager shared resource parameters. More... | |
Macros | |
| #define | UDMA_RM_RES_ID_INVALID ((uint32_t) 0xFFFF0005U) |
| Macro used to specify that Resource ID is invalid. More... | |
| #define | UDMA_RM_SHARED_RES_CNT_MIN ((uint32_t) 0xFFFF0006U) |
| Macro used to specify - reserve minimum required number of resources for an instance. More... | |
| #define | UDMA_RM_SHARED_RES_CNT_REST ((uint32_t) 0xFFFF0007U) |
| Macro used to specify - reserve all the remaining unreserved resources for an instance. More... | |
Functions | |
| Udma_RmSharedResPrms * | Udma_rmGetSharedResPrms (uint32_t instId, uint32_t resId) |
| Returns the RM Shared Resource default parameters structure for the requested resource. User can use this API to get the default parameters for a resource and override as per need. More... | |
UDMA RM related parameters and API.