UDMA proxy related parameters and API. More...
Go to the source code of this file.
Data Structures | |
| struct | Udma_ProxyCfg |
| This structure contains configuration parameters for each proxy thread. More... | |
| struct | Udma_ProxyHandle |
| UDMA proxy object. More... | |
Macros | |
| #define | UDMA_PROXY_INVALID ((uint16_t) 0xFFFFU) |
| Macro used to specify that proxy ID is invalid. More... | |
| #define | UDMA_PROXY_ANY ((uint16_t) 0xFFFEU) |
| Macro used to specify any available free proxy while requesting one. Used in the API Udma_proxyAlloc. More... | |
Functions | |
| int32_t | Udma_proxyAlloc (Udma_DrvHandle drvHandle, Udma_ProxyHandle proxyHandle, uint16_t proxyNum) |
| UDMA proxy allocation API. More... | |
| int32_t | Udma_proxyFree (Udma_ProxyHandle proxyHandle) |
| UDMA free proxy. More... | |
| int32_t | Udma_proxyConfig (Udma_ProxyHandle proxyHandle, const Udma_ProxyCfg *proxyCfg) |
| UDMA proxy config API. More... | |
| static void | Udma_proxyQueue (Udma_ProxyHandle proxyHandle, uint64_t phyDescMem) |
| UDMA queue descriptor to a proxy which is pre-configured to queue to a ring. More... | |
| static void | Udma_proxyDequeue (Udma_ProxyHandle proxyHandle, uint64_t *phyDescMem) |
| UDMA dequeue descriptor from a proxy which is pre-configured to dequeue from a ring. More... | |
| static void | Udma_proxyWrite64 (uintptr_t proxyAddr, uint64_t data) |
| API to write 64-bit data to proxy. More... | |
| static void | Udma_proxyRead64 (uintptr_t proxyAddr, uint64_t *data) |
| API to read 64-bit data from proxy. More... | |
UDMA proxy related parameters and API.