UDMA DRU related parameters and API. More...
Go to the source code of this file.
UDMA UTC Type | |
|
This represents the various types of UTC present in the SOC. | |
| #define | UDMA_UTC_TYPE_DRU (0U) |
| #define | UDMA_UTC_TYPE_DRU_VHWA (1U) |
| void | Udma_chDruSubmitTr (Udma_ChHandle chHandle, const CSL_UdmapTR *tr) |
| This API does a direct TR submission to the specified channel and core ID. More... | |
| uint32_t | Udma_druGetNumQueue (Udma_DrvHandle drvHandle, uint32_t utcId) |
| This API returns the number of queues present in a DRU. More... | |
| int32_t | Udma_druQueueConfig (Udma_DrvHandle drvHandle, uint32_t utcId, uint32_t queueId, const CSL_DruQueueConfig *queueCfg) |
| This API configures the DRU queue non-real time configurations. More... | |
| volatile uint64_t * | Udma_druGetTriggerRegAddr (Udma_ChHandle chHandle) |
| This API returns the software triggers register address for the DRU channel. More... | |
| void | UdmaDruQueueConfig_init (CSL_DruQueueConfig *queueCfg) |
| CSL_DruQueueConfig structure init function. More... | |
UDMA DRU related parameters and API.