VDEV structure. Must match with Linux. More...
#include <ipc_rsctypes.h>
Data Fields | |
| uint32_t | type |
| uint32_t | id |
| uint32_t | notifyid |
| uint32_t | dfeatures |
| uint32_t | gfeatures |
| uint32_t | config_len |
| uint8_t | status |
| uint8_t | num_of_vrings |
| uint8_t | reserved [2] |
VDEV structure. Must match with Linux.