This file contains the definition of all the message IDs, message formats to be able to interact with the System Controller firmware for OTP Key programming. More...
#include <stdint.h>Go to the source code of this file.
Functions | |
| int32_t | Sciclient_otpProcessKeyCfg (uint32_t *otpKeyCfgAddr, uint32_t timeout, uint32_t *debug_response) |
| Message to request a processor Provides a means for either the “recovery master” host or another host in the permitted access list to request for a physical processor control. More... | |
This file contains the definition of all the message IDs, message formats to be able to interact with the System Controller firmware for OTP Key programming.