PSDK QNX API Guide
ipc_virtio.h File Reference

VirtIO Interface for application. More...

#include <ti/drv/ipc/soc/ipc_soc.h>
#include <ti/drv/ipc/include/ipc_types.h>

Go to the source code of this file.

Data Structures

struct  Ipc_VirtIoParams
 Parameter structure for creating VirtIO table for each core combinations. More...
 

Functions

uint32_t Ipc_getVqObjMemoryRequired (void)
 Returns local memory for Virtio objects for all cores of SOC. More...
 
uint32_t Ipc_getVqObjMemoryRequiredPerCore (void)
 Returns local memory for Virtio objects for one core-pair. More...
 
int32_t Ipc_initVirtIO (Ipc_VirtIoParams *vqParam)
 Initailize the Virtio module. More...
 
int32_t Ipc_loadResourceTable (void *rsctable)
 Loads the resource table. If the remote core A72, and has valid radource table then, it will wait for Linux to be ready use address from resource table. More...
 
void * Ipc_getResourceTraceBufPtr (void)
 Gets the address of the trace buffer. More...
 
Bool Ipc_isRemoteReady (uint16_t procId)
 Checks if remote is ready. More...
 
int32_t Ipc_lateVirtioCreate (uint16_t procId)
 Creates Virtio late when Linux is ready. More...
 
Bool Ipc_isRemoteVirtioCreated (uint32_t remoteId)
 Check if a remote Virtio has been created. More...
 
void Ipc_resetCoreVirtIO (uint32_t remoteId)
 Resets the local VRing queue handles for the remote core. More...
 

Detailed Description

VirtIO Interface for application.