Files | |
| file | udma_utils.h |
| UDMA utility API to make TR, get TR descriptor memory requirement. | |
UDMA TR type | |
|
Various UDMA TR type supported | |
| uint32_t | UdmaUtils_getRingMemSize (uint8_t mode, uint32_t elemCnt, uint8_t elemSize) |
| UDMA get ring size utility API. More... | |
| static void | UdmaUtils_makeTrpd (void *pTrpd, uint32_t trType, uint32_t trCnt, uint32_t cqRingNum) |
| UDMA utility API to make TRPD. Other TRPD make APIs should be called only after this API. More... | |
| uint32_t | UdmaUtils_getTrSizeEncoded (uint32_t trType) |
| Returns the size of TR (encoded) based on the type. More... | |
| uint32_t | UdmaUtils_getTrSizeBytes (uint32_t trType) |
| Returns the size of TR in bytes based on the type. More... | |
| CSL_UdmapTR1 * | UdmaUtils_getTrpdTr1Pointer (uint8_t *trpdMem, uint32_t trIndex) |
| Returns the TR1 pointer in the TRPD memory based on the index. More... | |
| #define | UDMA_TR_TYPE_0 (CSL_UDMAP_TR_FLAGS_TYPE_1D_DATA_MOVE) |
| #define | UDMA_TR_TYPE_1 (CSL_UDMAP_TR_FLAGS_TYPE_2D_DATA_MOVE) |
| #define | UDMA_TR_TYPE_2 (CSL_UDMAP_TR_FLAGS_TYPE_3D_DATA_MOVE) |
| #define | UDMA_TR_TYPE_3 (CSL_UDMAP_TR_FLAGS_TYPE_4D_DATA_MOVE) |
| #define | UDMA_TR_TYPE_4 (CSL_UDMAP_TR_FLAGS_TYPE_4D_DATA_MOVE_FORMATTING) |
| #define | UDMA_TR_TYPE_5 (CSL_UDMAP_TR_FLAGS_TYPE_4D_CACHE_WARM) |
| #define | UDMA_TR_TYPE_8 (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE) |
| #define | UDMA_TR_TYPE_9 (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE_REPACKING) |
| #define | UDMA_TR_TYPE_10 (CSL_UDMAP_TR_FLAGS_TYPE_2D_BLOCK_MOVE) |
| #define | UDMA_TR_TYPE_11 (CSL_UDMAP_TR_FLAGS_TYPE_2D_BLOCK_MOVE_REPACKING) |
| #define | UDMA_TR_TYPE_15 (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE_REPACKING_INDIRECTION) |
| #define | UDMA_GET_TRPD_TR15_SIZE(n) (UDMA_ALIGN_SIZE(sizeof(CSL_UdmapTR15) + ((n) * (sizeof(CSL_UdmapTR15) + 4U)))) |
| UDMA TR15 packet descriptor memory size in bytes. This contains the CSL_UdmapCppi5TRPD + Padding to sizeof(CSL_UdmapTR15) + N* Type_15 TR (CSL_UdmapTR15) + N* TR response of 4 bytes. Since CSL_UdmapCppi5TRPD header is less than CSL_UdmapTR15, CSL_UdmapTR15 itself is used for size alignment. More... | |
| #define | UDMA_TR1_OFFSET (64U) |
| Offset for TR1 type TR from TRPD start address. More... | |
This is UDMA driver utilty parameters and API
| #define UDMA_TR_TYPE_0 (CSL_UDMAP_TR_FLAGS_TYPE_1D_DATA_MOVE) |
| #define UDMA_TR_TYPE_1 (CSL_UDMAP_TR_FLAGS_TYPE_2D_DATA_MOVE) |
| #define UDMA_TR_TYPE_2 (CSL_UDMAP_TR_FLAGS_TYPE_3D_DATA_MOVE) |
| #define UDMA_TR_TYPE_3 (CSL_UDMAP_TR_FLAGS_TYPE_4D_DATA_MOVE) |
| #define UDMA_TR_TYPE_4 (CSL_UDMAP_TR_FLAGS_TYPE_4D_DATA_MOVE_FORMATTING) |
| #define UDMA_TR_TYPE_5 (CSL_UDMAP_TR_FLAGS_TYPE_4D_CACHE_WARM) |
| #define UDMA_TR_TYPE_8 (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE) |
| #define UDMA_TR_TYPE_9 (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE_REPACKING) |
| #define UDMA_TR_TYPE_10 (CSL_UDMAP_TR_FLAGS_TYPE_2D_BLOCK_MOVE) |
| #define UDMA_TR_TYPE_11 (CSL_UDMAP_TR_FLAGS_TYPE_2D_BLOCK_MOVE_REPACKING) |
| #define UDMA_TR_TYPE_15 (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE_REPACKING_INDIRECTION) |
| #define UDMA_GET_TRPD_TR15_SIZE | ( | n | ) | (UDMA_ALIGN_SIZE(sizeof(CSL_UdmapTR15) + ((n) * (sizeof(CSL_UdmapTR15) + 4U)))) |
UDMA TR15 packet descriptor memory size in bytes. This contains the CSL_UdmapCppi5TRPD + Padding to sizeof(CSL_UdmapTR15) + N* Type_15 TR (CSL_UdmapTR15) + N* TR response of 4 bytes. Since CSL_UdmapCppi5TRPD header is less than CSL_UdmapTR15, CSL_UdmapTR15 itself is used for size alignment.
n - Number of TR's present in the TRPD
| #define UDMA_TR1_OFFSET (64U) |
Offset for TR1 type TR from TRPD start address.
| uint32_t UdmaUtils_getRingMemSize | ( | uint8_t | mode, |
| uint32_t | elemCnt, | ||
| uint8_t | elemSize | ||
| ) |
UDMA get ring size utility API.
| mode | [IN] Ring mode. Refer tisci_msg_rm_ring_cfg_req::mode |
| elemCnt | [IN] Ring element count. |
| elemSize | [IN] Ring element size. Refer Udma_RingElemSize |
|
inlinestatic |
UDMA utility API to make TRPD. Other TRPD make APIs should be called only after this API.
Note: This sets the most commonly used value for all the fields. User can override the fields after calling this API if required.
| pTrpd | [IN] Pointer to TRPD memory |
| trType | [IN] TR type. Refer Udma_TrType |
| trCnt | [IN] Number of TR entries present in the TRPD |
| cqRingNum | [IN] Completion ring number where the TRPD is returned after processing |
| uint32_t UdmaUtils_getTrSizeEncoded | ( | uint32_t | trType | ) |
Returns the size of TR (encoded) based on the type.
| trType | [IN] TR type. Refer Udma_TrType |
| uint32_t UdmaUtils_getTrSizeBytes | ( | uint32_t | trType | ) |
Returns the size of TR in bytes based on the type.
| trType | [IN] TR type. Refer Udma_TrType |
| CSL_UdmapTR1* UdmaUtils_getTrpdTr1Pointer | ( | uint8_t * | trpdMem, |
| uint32_t | trIndex | ||
| ) |
Returns the TR1 pointer in the TRPD memory based on the index.
| trpdMem | [IN] TRPD memory pointer |
| trIndex | [IN] Index to the TR to get the TR1 pointer address |