Files | |
| file | HwiP.h |
| Hardware Interrupt module for the RTOS Porting Interface. | |
Data Structures | |
| struct | HwiP_Params |
| Basic HwiP Parameters. More... | |
Macros | |
| #define | HWIP_USE_DEFAULT_PRIORITY (~((uint32_t)0)) |
Typedefs | |
| typedef void * | HwiP_Handle |
| Opaque client reference to an instance of a HwiP. More... | |
Enumerations | |
| enum | HwiP_Status { HwiP_OK = 0 , HwiP_FAILURE = (-(int32_t)1) } |
| Status codes for HwiP APIs. More... | |
Variables | |
| char * | HwiP_Params::name |
| uintptr_t | HwiP_Params::arg |
| uint32_t | HwiP_Params::priority |
| uint32_t | HwiP_Params::enableIntr |
| uint32_t | HwiP_Params::evtId |
Enumerates the types different trigger types. | |
| typedef uint32_t | OSAL_armGicTrigType_t |
| Enumerates the types different trigger types. Please refer to Section 4.3.13 Interrupt Configuration Registers, GICD_ICFGRn of ARM Generic Interrupt Controller Architecture version 2.0 Architecture Specification document for details. More... | |
| typedef void(* | HwiP_Fxn) (uintptr_t arg) |
| Prototype for the entry function for a hardware interrupt. More... | |
| typedef void(* | HwiP_DirectFxn) (void) |
| Prototype for the entry function for a hardware interrupt registered using HwiP_createDirect. More... | |
| void | HwiP_clearInterrupt (uint32_t interruptNum) |
| Function to clear a single interrupt. More... | |
| HwiP_Handle | HwiP_create (uint32_t interruptNum, HwiP_Fxn hwiFxn, const HwiP_Params *hwipParams) |
| Function to create an interrupt on CortexM devices. More... | |
| HwiP_Handle | HwiP_createDirect (uint32_t interruptNum, HwiP_DirectFxn hwiFxn, const HwiP_Params *hwipParams) |
| Function to create an interrupt using VIM direct registration. More... | |
| HwiP_Status | HwiP_delete (HwiP_Handle hwiPhandle) |
| Function to delete an interrupt on CortexM devices. More... | |
| uintptr_t | HwiP_disable (void) |
| Function to disable interrupts to enter a critical region. More... | |
| void | HwiP_disableInterrupt (uint32_t interruptNum) |
| Function to disable a single interrupt. More... | |
| void | HwiP_enableInterrupt (uint32_t interruptNum) |
| Function to enable a single interrupt. More... | |
| void | HwiP_Params_init (HwiP_Params *hwipParams) |
| Initialize params structure to default values. More... | |
| void | HwiP_restore (uintptr_t key) |
| Function to restore interrupts to exit a critical region. More... | |
| HwiP_Handle | HwiP_getHandle (uint32_t interruptNum) |
| Function to get HwiP Handle from an interrupt number. More... | |
| uint32_t | HwiP_getEventId (uint32_t interruptNum) |
| Function to get the eventId associated with an interrupt number. More... | |
| int32_t | HwiP_post (uint32_t interruptNum) |
| Function to post the Hwi interrupt by software. More... | |
| #define | OSAL_ARM_GIC_TRIG_TYPE_LEVEL ((uint32_t) 1U) |
| #define | OSAL_ARM_GIC_TRIG_TYPE_EDGE ((uint32_t) 2U) |
| #define | OSAL_ARM_GIC_TRIG_TYPE_HIGH_LEVEL ((uint32_t) 3U) |
| #define | OSAL_ARM_GIC_TRIG_TYPE_LOW_LEVEL ((uint32_t) 4U) |
| #define | OSAL_ARM_GIC_TRIG_TYPE_RISING_EDGE ((uint32_t) 5U) |
| #define | OSAL_ARM_GIC_TRIG_TYPE_FALLING_EDGE ((uint32_t) 6U) |
HWIP interface
| #define HWIP_USE_DEFAULT_PRIORITY (~((uint32_t)0)) |
| #define OSAL_ARM_GIC_TRIG_TYPE_LEVEL ((uint32_t) 1U) |
Corresponding interrupt is edge sensitive
| #define OSAL_ARM_GIC_TRIG_TYPE_EDGE ((uint32_t) 2U) |
Coressponding interrupt is high level sensitive
| #define OSAL_ARM_GIC_TRIG_TYPE_HIGH_LEVEL ((uint32_t) 3U) |
Coressponding interrupt is low level sensitive
| #define OSAL_ARM_GIC_TRIG_TYPE_LOW_LEVEL ((uint32_t) 4U) |
Coressponding interrupt is rising edge sensitive
| #define OSAL_ARM_GIC_TRIG_TYPE_RISING_EDGE ((uint32_t) 5U) |
Coressponding interrupt is falling edge sensitive
| #define OSAL_ARM_GIC_TRIG_TYPE_FALLING_EDGE ((uint32_t) 6U) |
| typedef void* HwiP_Handle |
Opaque client reference to an instance of a HwiP.
A HwiP_Handle returned from the HwiP_create represents that instance.
| typedef uint32_t OSAL_armGicTrigType_t |
Enumerates the types different trigger types. Please refer to Section 4.3.13 Interrupt Configuration Registers, GICD_ICFGRn of ARM Generic Interrupt Controller Architecture version 2.0 Architecture Specification document for details.
Corresponding interrupt is level sensitive
| typedef void(* HwiP_Fxn) (uintptr_t arg) |
Prototype for the entry function for a hardware interrupt.
| typedef void(* HwiP_DirectFxn) (void) |
Prototype for the entry function for a hardware interrupt registered using HwiP_createDirect.
| enum HwiP_Status |
| void HwiP_clearInterrupt | ( | uint32_t | interruptNum | ) |
Function to clear a single interrupt.
| interruptNum | interrupt number to clear |
| HwiP_Handle HwiP_create | ( | uint32_t | interruptNum, |
| HwiP_Fxn | hwiFxn, | ||
| const HwiP_Params * | hwipParams | ||
| ) |
Function to create an interrupt on CortexM devices.
| interruptNum | Interrupt Vector Id |
| hwiFxn | entry function of the hardware interrupt |
| hwipParams | Pointer to the instance configuration parameters. NULL denotes to use the default parameters. The HwiP default parameters are noted in HwiP_Params_init. |
| HwiP_Handle HwiP_createDirect | ( | uint32_t | interruptNum, |
| HwiP_DirectFxn | hwiFxn, | ||
| const HwiP_Params * | hwipParams | ||
| ) |
Function to create an interrupt using VIM direct registration.
| interruptNum | Interrupt Vector Id |
| hwiFxn | entry function of the hardware interrupt |
| hwipParams | Pointer to the instance configuration parameters. NULL denotes to use the default parameters. The HwiP default parameters are noted in HwiP_Params_init. |
| HwiP_Status HwiP_delete | ( | HwiP_Handle | hwiPhandle | ) |
Function to delete an interrupt on CortexM devices.
| hwiPhandle | returned from the HwiP_create call |
| uintptr_t HwiP_disable | ( | void | ) |
Function to disable interrupts to enter a critical region.
This function can be called multiple times.
For Non-OS case, it must unwound in the reverse order. For example
For FreeRTOS case, after the schedular had started the kernel keeps track of critical nesting count. So here the return key will be NULL.
| void HwiP_disableInterrupt | ( | uint32_t | interruptNum | ) |
Function to disable a single interrupt.
| interruptNum | interrupt number to disable |
| void HwiP_enableInterrupt | ( | uint32_t | interruptNum | ) |
Function to enable a single interrupt.
| interruptNum | interrupt number to enable |
| void HwiP_Params_init | ( | HwiP_Params * | hwipParams | ) |
Initialize params structure to default values.
The default parameters are:
| hwipParams | Pointer to the instance configuration parameters. |
| void HwiP_restore | ( | uintptr_t | key | ) |
Function to restore interrupts to exit a critical region.
| key | return from HwiP_disable |
| HwiP_Handle HwiP_getHandle | ( | uint32_t | interruptNum | ) |
Function to get HwiP Handle from an interrupt number.
| interruptNum | the interrupt number |
| uint32_t HwiP_getEventId | ( | uint32_t | interruptNum | ) |
Function to get the eventId associated with an interrupt number.
| interruptNum | the interrupt number |
| int32_t HwiP_post | ( | uint32_t | interruptNum | ) |
Function to post the Hwi interrupt by software.
| interruptNum | the interrupt number |
| char* HwiP_Params::name |
Name of the clock instance. Memory must persist for the life of the clock instance. This can be used for debugging purposes, or set to NULL if not needed.
| uintptr_t HwiP_Params::arg |
Argument passed into the Hwi function.
| uint32_t HwiP_Params::priority |
Device specific priority. Note: For R5 Core, baremetal case, there is no device specific priority set - all interrupts are handled at the same priority. So, this is not applicable for bare metal R5 Core interrupt config
| uint32_t HwiP_Params::enableIntr |
When set to TRUE, interrupt is enabled after the create otherwise interrupt is disabled after HwiP_Create
| uint32_t HwiP_Params::evtId |
Event Id associated