PSDK QNX API Guide
RegisterIntr.h File Reference

Interrupt register routines. More...

#include <ti/osal/EventCombinerP.h>
#include <ti/osal/HwiP.h>
#include <ti/osal/MuxIntcP.h>
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>

Go to the source code of this file.

Data Structures

struct  OsalRegisterIntParams_corepac_t
 Interrupt Configuration parameters for the corepac (c6x/a15/m5/a8/a9) More...
 
struct  OsalRegisterIntParams_socmux_t
 Interrupt Configuration parameters for soc mux prior to reaching the core. More...
 
struct  OsalRegisterIntrParams_t
 Interrupt Configuration parameters This is the data structure used to configure the interrupts in the system. coreConfig: This part configures the interrupt for corepac such as c66x, arm, m4 socMuxConfig: This part configures the interrupt path for any SOC level mux such as CIC/GIC or cross bar, leading up to the corepac. More...
 

Macros

#define OSAL_REGINT_INTVEC_EVENT_COMBINER   (16U)
 For C6x, if intVec=16, then event combiner is to be used. More...
 

Typedefs

typedef void(* Osal_IsrRoutine) (uintptr_t arg)
 

Osal Interrupt return Codes

#define OSAL_INT_SUCCESS   ((int32_t) 0)
 
#define OSAL_INT_ERR_INVALID_PARAMS   ((int32_t) -1)
 
#define OSAL_INT_ERR_HWICREATE   ((int32_t) -2)
 
#define OSAL_INT_ERR_EVENTCOMBINER_REG   ((int32_t) -3)
 
#define OSAL_INT_ERR_DELETE   ((int32_t) -4)
 
#define OSAL_INT_UNSUPPORTED   ((int32_t) -5)
 
typedef int32_t OsalInterruptRetCode_e
 Return error codes for Osal Interrupt functions. More...
 
void Osal_RegisterInterrupt_initParams (OsalRegisterIntrParams_t *interruptRegParams)
 Function to initialize the interrupt registration configuration data structure. More...
 
OsalInterruptRetCode_e Osal_RegisterInterruptDirect (OsalRegisterIntrParams_t *interruptRegParams, HwiP_DirectFxn isrFxn, HwiP_Handle *hwiPHandlePtr)
 Function to register direct interrupt with parameters provided. More...
 
OsalInterruptRetCode_e Osal_RegisterInterrupt (OsalRegisterIntrParams_t *interruptRegParams, HwiP_Handle *hwiPHandlePtr)
 Function to register interrupt with parameters provided. More...
 
OsalInterruptRetCode_e Osal_DeleteInterrupt (HwiP_Handle hwiPhandle, uint32_t corepacEventNum)
 Function to delete interrupt corresponding to an event number. More...
 
void Osal_EnableInterrupt (uint32_t corepacEvent, uint32_t interruptNum)
 Function to enable the interrupt corresponding to an event number. More...
 
void Osal_DisableInterrupt (uint32_t corepacEvent, uint32_t interruptNum)
 Function to disable the interrupt corresponding to an event number. More...
 
void Osal_ClearInterrupt (uint32_t corepacEvent, uint32_t interruptNum)
 Function to clear the interrupt corresponding to an event number. More...
 

Detailed Description

Interrupt register routines.

============================================================================