Basic ClockP Parameters. More...
#include <ClockP.h>
Data Fields | |
| void * | pErrBlk |
| uint8_t | startMode |
| uint32_t | period |
| uint8_t | runMode |
| void * | arg |
Basic ClockP Parameters.
Structure that contains the parameters are passed into ClockP_create when creating a ClockP instance.