Hardware Interrupt module for the RTOS Porting Interface. More...
#include <stdint.h>#include <stdbool.h>#include <stddef.h>Go to the source code of this file.
Data Structures | |
| struct | HwiP_Params |
| Basic HwiP Parameters. More... | |
Macros | |
| #define | HWIP_USE_DEFAULT_PRIORITY (~((uint32_t)0)) |
Typedefs | |
| typedef void * | HwiP_Handle |
| Opaque client reference to an instance of a HwiP. More... | |
Enumerations | |
| enum | HwiP_Status { HwiP_OK = 0 , HwiP_FAILURE = (-(int32_t)1) } |
| Status codes for HwiP APIs. More... | |
Enumerates the types different trigger types. | |
| #define | OSAL_ARM_GIC_TRIG_TYPE_LEVEL ((uint32_t) 1U) |
| #define | OSAL_ARM_GIC_TRIG_TYPE_EDGE ((uint32_t) 2U) |
| #define | OSAL_ARM_GIC_TRIG_TYPE_HIGH_LEVEL ((uint32_t) 3U) |
| #define | OSAL_ARM_GIC_TRIG_TYPE_LOW_LEVEL ((uint32_t) 4U) |
| #define | OSAL_ARM_GIC_TRIG_TYPE_RISING_EDGE ((uint32_t) 5U) |
| #define | OSAL_ARM_GIC_TRIG_TYPE_FALLING_EDGE ((uint32_t) 6U) |
| typedef uint32_t | OSAL_armGicTrigType_t |
| Enumerates the types different trigger types. Please refer to Section 4.3.13 Interrupt Configuration Registers, GICD_ICFGRn of ARM Generic Interrupt Controller Architecture version 2.0 Architecture Specification document for details. More... | |
| typedef void(* | HwiP_Fxn) (uintptr_t arg) |
| Prototype for the entry function for a hardware interrupt. More... | |
| typedef void(* | HwiP_DirectFxn) (void) |
| Prototype for the entry function for a hardware interrupt registered using HwiP_createDirect. More... | |
| void | HwiP_clearInterrupt (uint32_t interruptNum) |
| Function to clear a single interrupt. More... | |
| HwiP_Handle | HwiP_create (uint32_t interruptNum, HwiP_Fxn hwiFxn, const HwiP_Params *hwipParams) |
| Function to create an interrupt on CortexM devices. More... | |
| HwiP_Handle | HwiP_createDirect (uint32_t interruptNum, HwiP_DirectFxn hwiFxn, const HwiP_Params *hwipParams) |
| Function to create an interrupt using VIM direct registration. More... | |
| HwiP_Status | HwiP_delete (HwiP_Handle hwiPhandle) |
| Function to delete an interrupt on CortexM devices. More... | |
| uintptr_t | HwiP_disable (void) |
| Function to disable interrupts to enter a critical region. More... | |
| void | HwiP_disableInterrupt (uint32_t interruptNum) |
| Function to disable a single interrupt. More... | |
| void | HwiP_enableInterrupt (uint32_t interruptNum) |
| Function to enable a single interrupt. More... | |
| void | HwiP_Params_init (HwiP_Params *hwipParams) |
| Initialize params structure to default values. More... | |
| void | HwiP_restore (uintptr_t key) |
| Function to restore interrupts to exit a critical region. More... | |
| HwiP_Handle | HwiP_getHandle (uint32_t interruptNum) |
| Function to get HwiP Handle from an interrupt number. More... | |
| uint32_t | HwiP_getEventId (uint32_t interruptNum) |
| Function to get the eventId associated with an interrupt number. More... | |
| int32_t | HwiP_post (uint32_t interruptNum) |
| Function to post the Hwi interrupt by software. More... | |
Hardware Interrupt module for the RTOS Porting Interface.
============================================================================
The HwiP_disable/HwiP_restore APIs can be called recursively. The order of the HwiP_restore calls, must be in reversed order. For example: