UDMA event related parameters. More...
#include <udma_event.h>
Data Fields | |
| uint32_t | eventType |
| uint32_t | eventMode |
| Udma_ChHandle | chHandle |
| Udma_RingHandle | ringHandle |
| Udma_EventHandle | masterEventHandle |
| Udma_EventCallback | eventCb |
| uint32_t | intrPriority |
| void * | appData |
| uint32_t | osalRegisterDisable |
| uint32_t | preferredCoreIntrNum |
| Udma_RingMonHandle | monHandle |
| volatile uint64_t * | intrStatusReg |
| volatile uint64_t * | intrClearReg |
| uint64_t | intrMask |
| uint32_t | vintrNum |
| uint32_t | coreIntrNum |
UDMA event related parameters.
Requirement: DOX_REQ_TAG(PDK-2628), DOX_REQ_TAG(PDK-2627) DOX_REQ_TAG(PDK-2626), DOX_REQ_TAG(PDK-2625)