PSDK QNX API Guide
TaskP_Params Struct Reference

Basic TaskP Parameters. More...

#include <TaskP.h>

Data Fields

const char * name
 
int8_t priority
 
uint8_t padding1
 
uint16_t padding2
 
uint32_t stacksize
 
void * pErrBlk
 
void * arg0
 
void * arg1
 
void * stack
 
void * userData
 
TaskP_Privilege_Mode taskPrivilege
 

Detailed Description

Basic TaskP Parameters.

Structure that contains the parameters are passed into TaskP_create when creating a TaskP instance.


The documentation for this struct was generated from the following file: