IPC Low Level Driver API/interface data types file. More...
#include <ti/csl/soc.h>#include <ti/csl/csl_types.h>#include <ti/drv/ipc/include/ipc_types.h>#include <ti/drv/ipc/include/ipc_rsctypes.h>#include <ti/drv/ipc/include/ipc_config.h>#include <ti/drv/ipc/include/ipc_mp.h>#include <ti/drv/ipc/include/ipc_virtio.h>#include <ti/drv/ipc/soc/ipc_soc.h>#include <string.h>Go to the source code of this file.
Data Structures | |
| struct | Ipc_InitPrms |
| IPC initialization parameters. More... | |
| struct | RPMessage_Params |
| Parameter structure for creating RPMessage endpoints. More... | |
Typedefs | |
| typedef struct RPMessage_Object_s * | RPMessage_Handle |
| RPMessage_Handle type. More... | |
| typedef void(* | RPMessage_Callback) (RPMessage_Handle handle, void *arg, void *data, uint16_t len, uint32_t src) |
| RPMessage_Callback. More... | |
Functions | |
| void | IpcInitPrms_init (uint32_t instId, Ipc_InitPrms *initPrms) |
| Initialize IPC init params. More... | |
| int32_t | Ipc_init (const Ipc_InitPrms *cfg) |
| Initialize IPC module. More... | |
| int32_t | Ipc_deinit (void) |
| De Initialize IPC module. More... | |
| uint32_t | RPMessage_getMessageBufferSize (void) |
| Returns Message Buffer Size. More... | |
| uint32_t | RPMessage_getObjMemRequired (void) |
| Returns local memory for RPMessage Object. More... | |
| int32_t | RPMessage_init (RPMessage_Params *params) |
| Initialize RPMessage Module. More... | |
| void | RPMessage_deInit (void) |
| Tear down the RPMessage Module. The module API should not be used after this is called. More... | |
| int32_t | RPMessageParams_init (RPMessage_Params *params) |
| Initialize an RPMessage_Params structure to default values. More... | |
| RPMessage_Handle | RPMessage_create (RPMessage_Params *params, uint32_t *endPt) |
| Create a endpoint instance for receiving. More... | |
| int32_t | RPMessage_setCallback (RPMessage_Handle handle, RPMessage_Callback cb, void *arg) |
| Sets callback. More... | |
| int32_t | RPMessage_recv (RPMessage_Handle handle, void *data, uint16_t *len, uint32_t *rplyEndPt, uint32_t *fromProcId, uint32_t timeout) |
| Receives a message from an endpoint instance. More... | |
| int32_t | RPMessage_recvNb (RPMessage_Handle handle, void *data, uint16_t *len, uint32_t *rplyEndPt, uint32_t *fromProcId) |
| A non blocking API to receive message. More... | |
| int32_t | RPMessage_send (RPMessage_Handle handle, uint32_t dstProc, uint32_t dstEndPt, uint32_t srcEndPt, void *data, uint16_t len) |
| Sends data to a remote processor. More... | |
| int32_t | RPMessage_delete (RPMessage_Handle *handlePtr) |
| Delete an endpoint instance. More... | |
| void | RPMessage_unblock (RPMessage_Handle handle) |
| Unblocks an RPMessage_recv() More... | |
| int32_t | RPMessage_getRemoteEndPt (uint32_t currProcId, const char *name, uint32_t *remoteProcId, uint32_t *remoteEndPt, uint32_t timeout) |
| Wait for an endpoint to become available on another processor. More... | |
| int32_t | RPMessage_getRemoteEndPtToken (uint32_t currProcId, const char *name, uint32_t *remoteProcId, uint32_t *remoteEndPt, uint32_t timeout, uint32_t token) |
| void | RPMessage_unblockGetRemoteEndPt (uint32_t token) |
| Unblocks an RPMessage_getRemoteEndPtToken() call. More... | |
| int32_t | RPMessage_announce (uint32_t remoteProcId, uint32_t endPt, const char *name) |
| Annouce the name of an endpoint and that it is ready to to receive messages. More... | |
| void | Ipc_mailboxEnableNewMsgInt (uint16_t selfId, uint16_t remoteProcId) |
| API Mailbox Enable new MSG interrupt for a given remote processor. More... | |
| void | Ipc_mailboxDisableNewMsgInt (uint16_t selfId, uint16_t remoteProcId) |
| API Mailbox Disable new MSG interrupt for a given remote processor. More... | |
IPC Low Level Driver API/interface data types file.