2.2. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layersetup.sh -f <config>
The following config files are located in the configs/psdkla
directory of the configs directory.
Config File | Description | Supported machines |
---|---|---|
psdkla-06_01_00_05.txt | Processor SDK Linux Automotive 06_01_00_05 Release | j7-evm |