2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) for Linux Automotive provides a fundamental software platform for development, deployment and execution of Linux based applications and includes the following:
- Bootloaders, Linux Kernel & Filesystem
- SDK installer
- Setup scripts
- Demo applications
- Documentation
Note
For building some of the RTOS-based demonstrations, you should also download Processor SDK RTOS Automotive (PSDKRA) installer. For more information, refer to <PSDKRA install path>/index.html.
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see Processor SDK Linux GPLv3 Disclaimer.
2.1.3. Documentation¶
- Processor SDK Linux Software Developer’s Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Linux release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Processor SDK Linux Getting Started Guide: Provides information on getting the software and running examples/demonstrations bundled in the SDK.
- Software Manifest: Provides license information on software
included in the SDK release. This document is in the release at
[INSTALL-DIR]/docs
. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Supported Platforms¶
See here for a list of supported platforms and links to more information.
2.1.5. Release 06.02.00¶
Released February 2020
2.1.5.1. What’s New¶
- A72 PMU support for Performance profiling
- IO Hub: PCIe Backplane demonstration using camera data
2.1.5.2. Release features¶
- R5 SPL:
- Early booting of MCU R5F and MainSS R5F’s
- Bootstrapping 2nd stage boot loader (u-boot) on A72
- Hyperflash support, UART boot, OSPI boot support.
- eMMC HS400 mode support
- eMMC boot support
- A72 U-boot:
- Early booting of remote cores (C7x, C66x, Main subsystem R5F’s) with configurable order of boot-strapping
- Support for booting both compressed and uncompressed kernel image
- Basic HYP mode support - boots up uboot in EL2 privileged mode
- Hyperflash support, OSPI support, MMCSD support
- SD card boot, hyperflash boot support
- USB Host and mass storage support
- Support for DFU download to SD card, eMMC, OSPI
- UFS support
- eMMC boot support
- Kernel: Kernel image includes support for the following drivers
- MMC support
- I2C support
- CPSW2G Ethernet driver
- UART driver, UART console support
- USB driver with support for device/host mode of operation
- PCIe Root Complex and Endpoint drivers
- CPSW9G Virtual driver
- USB gadget driver support
- Composite device
- Multifunction composite device
- USB DRD dual role support
- Support for dual voltage SD cards (UHS mode)
- PCIe backplane support
- PCIe Gen3 2xlane support
- eMMC HS400 speed mode support
- UART DMA mode support
- UFS support
- ADC basic functionality
- Crypto acceleration support for AES, 3-DES, and RNG
- Graphics:
- Support for OpenGL ® ES 1.x, OpenGL ® ES 2.0 and OpenGL ® ES 3.2 APIs
- Weston window composition with GPU acceleration support
- DRM-based display backend
- Offscreen rendering mode support
- DMABUF buffer import support
- Support for YUV texture formats
- Support for GPU profiling tools (PVRTrace and PVRTune)
- IPC:
- IPC support between
- A72 to C7x
- A72 to each C66x core
- A72 to each MainSS R5F core
- A72 to each MCU island R5F core
- Support for IPC in both IPC-only mode (core loaded by u-boot) and remoteproc mode (core loaded by Linux Kernel)
- Mailbox and H/W spinlock support
- IPC support between
- Multimedia:
- Decoder:
- Gstreamer-based video decode plugin for H.264 & H.265/HEVC formats
- Support for decode resolutions up to 4K@60fps
- Support for decoding NV12/NV16 pixel formats
- Support for 8-bit and 10-bit pixel depths
- Support for decoding streams with ‘B’ Frames
- Support for multi channel decoding in driver and gstreamer
- Support for MJPEG and JPEG Image decoder
- Gstreamer plugin support for wayland sink
- Support for video decoder error recovery
- Support for interlaced video decode
- Encoder:
- Driver support for H.264 video encoder with NV12, 8 bit content
- Driver support for multi channel encoding
- Decoder:
- Display:
- DSS support for cropping, scaling, gamma correction, per-pixel blending and global alpha blending
- DSS support for Color Space Conversion (CSC) and Color Phase Rotation (CPR)
- DRM API support
- Support for NV12, UYVY, and XRGB888 data
- Static partitioning of DSS resources and using video pipelines on shared videoport
- Audio:
- Audio playback and Audio record support at 48 KHz, 24 bits per sample
- Stereo and Multichannel support
- Multi-codec support
- McASP: Master and slave mode support
- Multi-codec support with separate serializer per codec
- Virtualisation:
- Jailhouse hypervisor support
- Static system partitioning: SD/eMMC, Display pipes, sproxy threads, UARTs, etc.
- IO isolation between VMs
- PVU and SMMU backed IO isolation support
- SMMU emulation in Jailhouse hypervisor
2.1.5.3. Component versions¶
component | source | branch | version |
---|---|---|---|
arm-trusted-firmware | git://git.ti.com/atf/arm-trusted-firmware.git | ti-atf | e516a389ac12fbe1597f61fea80ed3f230b9c5fd |
optee-os | git://git.ti.com/optee/ti-optee-os.git | ti-optee-os | 5208e5c1f3743fcde71e150eada2fc9945f749df |
U-boot | git://git.ti.com/ti-u-boot/ti-u-boot.git | ti-u-boot-2019.01 | 350f3927b89bc06ce1c9ddb618280d298c418b94 |
Linux Kernel | git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git | ti-linux-4.19.y | 5a23bc00e08d26bb83952953d909c95b42fab70c |
Jailhouse | git://git.ti.com/jailhouse/ti-jailhouse.git | ti-jailhouse-0.10 | b3a68ac89d7ed955546eae91954b184ec1583ce3 |
2.1.6. Issues Tracker¶
2.1.6.1. Issues fixed in this release¶
Record ID | Summary |
---|---|
LCPD-16024 | DSS7: Driver does not check for unsupported pixel clock as per HW limit |
LCPD-16121 | DP: Videomodes that exceed the link bandwidth need to be rejected |
LCPD-16599 | WIZ driver memleak on module unload |
LCPD-16610 | DP driver reports “No supported color_format found” |
LCPD-16641 | tidss: need to ensure the output width is divisible by 2 |
LCPD-16840 | DP driver error handling is missing proper cleanups |
LCPD-17084 | tidss: page-flip race issue |
LCPD-17201 | tidss compilation warnings with W=1 |
LCPD-17253 | g_multi seems hanging when usbdev is full-speed/high-speed |
LCPD-17292 | CDC ACM has problem after multiple modprobe |
LCPD-17300 | J7: possible memleak in DP PHY driver |
LCPD-17301 | J7: possible memleak in tidss driver |
LCPD-17316 | U-boot: J7es: gpios above 32 don’t work with the da8xx_gpio.c driver |
LCPD-17347 | PCIe: RC: With SMMU disabled, SSD partitions are not mounted |
LCPD-17363 | tidss: Default premultiplied alpha configuration is broken |
LCPD-17378 | spl-dfu boot does not work using 2019.05 |
LCPD-17379 | J7 Alpha board can’t boot from 8G Sandisk SD cards (16G+ works) |
LCPD-17380 | usb: g_ncm: USBDEV is not at superspeed |
LCPD-17402 | PAT: kmemleak with sg tables |
LCPD-17407 | DP: race issue when enabling the DP output |
LCPD-17411 | Kernel ‘perf’ output data broken |
LCPD-17439 | Seeing i2c_write error with sysfw |
LCPD-17470 | CPSW: Still seeing multicast packets with promisc and allmulti disabled |
LCPD-17524 | USBDev: g_cdc does not work at superspeed |
LCPD-17542 | j721e: custom audio support dts changes missing for alpha board |
LCPD-17566 | J7es does not boot from some SD cards |
LCPD-17672 | MMC: Some cards fail to tune in DDR50 speed mode |
LCPD-17833 | CPSW2G: vlan max_size (>1518) packet drop after interface down/up |
LCPD-17835 | ntb_hw_epf: probe failed with error -5 |
LCPD-17905 | j721e: QSPI_S_PERF_RAW_READ test failed |
LCPD-17912 | CPSW9G: Cannot bring up interface over NFS or SD Boot |
PSDKLA-5002 | Video playback crashes on continuous playback with VM |
2.1.6.2. Errata workarounds¶
None
2.1.6.3. Open Defects¶
Record ID | Summary | Workaround |
---|---|---|
LCPD-16120 | DP: Link fails right after link training, unless voltage swing is 2 or 3 | |
LCPD-16130 | Exception triggered by drm_dev_unregister during poweroff | |
LCPD-16208 | FIFO Underflows during video playback on 4k panel | |
LCPD-16366 | RGX kick test fails when 32 sync dependencies are set for each command | |
LCPD-16505 | Wrong clock rate is reported for 157:400, 157:401 (HSDIVIDER after PLL4 and 15) | |
LCPD-16531 | video decode: vxd_dec warnings displayed at end of gstreamer hevc playback to kmssink for certain video | |
LCPD-16535 | remoteproc/k3-dsp: PDK IPC echo test binaries fails to do IPC in remoteproc mode on second run | |
LCPD-16545 | remoteproc/k3-r5f: PDK IPC echo_test image fails to boot up in remoteproc mode on second run | |
LCPD-16591 | PCIe wifi ping stress test failed | |
LCPD-16616 | Jailhouse: Failure in mhdp probe while restarting the Linux VM | |
LCPD-16628 | Could not enumerate PLEXTOR pcie SSD | |
LCPD-16640 | PCIe RC: GIC ITS misbehaves when more than 4 devices use it simultaneously | |
LCPD-16836 | DP: GeChic display EDID read failures | |
LCPD-16921 | GPU driver doesn’t unregister genpd name on unload | |
LCPD-17006 | 4k DP Display Shows Blank Screen sometimes when booting | |
LCPD-17010 | J7ES: USB: gadget mode breaks with PC host with USB3.0 LPM | |
LCPD-17171 | Uboot dhcp occasionally failed | |
LCPD-17213 | Weston sometimes fails to start when booting with nfs filesystem | |
LCPD-17229 | vxd_dec: kernel crash if rootfs has no pvdec_full_bin.fw firmware file | |
LCPD-17236 | PDK-IPC build from sources is not creating stripped images and links | |
LCPD-17284 | remoteproc/k3-r5: Cores are started out-of-order when core 0 file size >> core 1 file size | |
LCPD-17381 | J7 Beta board ti_sci_power_domain_on: get_device(91) failed (-19) | |
LCPD-17387 | Underflow and CRTC SYNC LOST observed while running GLMark2 (1x1080p + 1x4k) | |
LCPD-17398 | J7 Beta board hangs and cannot power cycle via automation interface | |
LCPD-17403 | PAT: DMA-API warning | |
LCPD-17406 | U-boot: Uboot has no knowledge of memory reserved for remote cores | |
LCPD-17418 | J7 sometimes failed to boot | Flash firmware into mmc rootfs |
LCPD-17421 | CPSW9G: Can’t bring up interface over NFS | |
LCPD-17543 | Some cpuhotplug tests failed | |
LCPD-17673 | No software documentation for the Timer module | |
LCPD-17770 | U-Boot: Fix order of MCU R5 shutdown depending on cluster mode | |
LCPD-17771 | cryptomgr_test kmemleak | |
LCPD-17772 | systemd doesn’t show ansi sequences correctly | |
LCPD-17773 | cryptomgr_test related DMA-API errors | |
LCPD-17780 | Mbox timedout in resp | |
LCPD-17789 | UBOOT J7: Could not see UFS device by scsi scan | |
LCPD-17794 | ext4write failed to write firmware to SD card | |
LCPD-17798 | 2020 LTS: INTA/INTR smp_affinity failure and IRQ allocation issues. | |
LCPD-17814 | Kingston 16G card could not boot to uboot prompt | |
LCPD-18056 | PVR errors observed while running graphics tests | |
LCPD-18061 | Linux boot writes login prints to other UART ports that it doesn’t own | |
LCPD-18062 | tidss: OVR registerhandlig code is naive, and fails in complex cases |
2.1.6.4. Known issues & limitations¶
Record ID | Summary | Workaround |
---|---|---|
LCPD-16396 | J721E: RC: Unsupported request in configuration completion packets results in an abort | Workaround for Multifunction: Configure all the physical functions supported by the endpoint. |
Installation and Usage
The Software Developer’s Guide provides instructions on how to setup your Linux development environment, install the SDK and start your development. It also includes User’s Guides for various Example Applications.
Host Support
For the specific supported hosts for current SDK, see Supported Platforms.
Note
Processor SDK Installer is 64-bit, and installs only on 64-bit host machine. Support for 32-bit host is dropped as Linaro toolchain is available only for 64-bit machines.