3.1.1.9. UART
This section documents how to use the UART to load files to boot the board into U-Boot. After that the user is expected to know how they want to continue loading files.
3.1.1.9.1. Booting U-Boot from the console UART
In some cases we support loading SPL and U-Boot over the console UART.
You will need to use the tiboot3.bin, tispl.bin and u-boot.img
files to boot. As per the TRM, the file is to be loaded via the X-MODEM
protocol at 115200 baud 8 stop bits no parity (same as using it for
console). SPL in turn expects to be sent u-boot.img at the same rate
but via Y-MODEM. An example session from the host PC, assuming console
is on ttyUSB0 and already configured would be and the lrzsz package
is installed
WHO |
Loading WHAT |
HW Module |
Protocol |
|---|---|---|---|
Boot ROM |
tiboot3.bin |
MCU_UART0 |
X-Modem |
R5 SPL |
tispl.bin |
MAIN_UART0 |
Y-Modem |
A53/A72 SPL |
u-boot.img |
MAIN_UART0 |
Y-Modem |
UART_BOOT_MAIN_UART and UART_BOOT_MCU_UART should be set to serial ports such as /dev/ttyUSBx.
$ sb --xmodem $OUT_R5/tiboot3.bin > $UART_BOOT_MCU_UART < $UART_BOOT_MCU_UART
$ sb --ymodem $OUT_AXX/tispl.bin > $UART_BOOT_MAIN_UART < $UART_BOOT_MAIN_UART
$ sb --ymodem $OUT_AXX/u-boot.img > $UART_BOOT_MAIN_UART < $UART_BOOT_MAIN_UART