5. Demo Applications

The SDK supports the following Out-Of-Box demo-applications

Use the tisdk-default-image-am69-sk to be able to run the above demo applications.

  • Refer to Hardware EVM Setup for preliminary hardware setup.

  • Refer to Create SD Card to prepare a SD card with the tisdk-default-image provided in the SDK.

  • To run a demo refer to the respective user guide from above