VISS Module Data Structure.
Contains the data objects required to use tivxVpacVissNode
Data Fields | |
| vx_node | node |
| vx_user_data_object | config |
| tivx_vpac_viss_params_t | params |
| vx_user_data_object | dcc_config |
| vx_object_array | output_arr |
| vx_object_array | h3a_stats_arr |
| vx_int32 | en_out_viss_write |
| vx_node | img_write_node |
| vx_node | h3a_write_node |
| vx_array | file_path |
| vx_array | img_file_prefix |
| vx_array | h3a_file_prefix |
| vx_user_data_object | write_cmd |
| vx_char | output_file_path [APP_MODULES_MAX_OBJ_NAME_SIZE] |
| vx_char | obj_name [APP_MODULES_MAX_OBJ_NAME_SIZE] |
| vx_node VISSObj::node |
VISS node object
| vx_user_data_object VISSObj::config |
User data object for config parameter, used as node parameter of VISS node
| tivx_vpac_viss_params_t VISSObj::params |
VISS node params structure to initialize config object
| vx_user_data_object VISSObj::dcc_config |
User data object for DCC parameter, used as node parameter of VISS node
| vx_object_array VISSObj::output_arr |
Object array of output images, used as node parameter of VISS node
| vx_object_array VISSObj::h3a_stats_arr |
Object array of H3A objects, used as node parameter of VISS node
| vx_int32 VISSObj::en_out_viss_write |
Flag to indicate whether or not the intermediate output is written
| vx_node VISSObj::img_write_node |
Node used to write VISS output
| vx_node VISSObj::h3a_write_node |
Node used to write H3A output
| vx_array VISSObj::file_path |
File path used to write VISS node output
| vx_array VISSObj::img_file_prefix |
File path prefix used to write VISS output
| vx_array VISSObj::h3a_file_prefix |
File path prefix used to write H3A output
| vx_user_data_object VISSObj::write_cmd |
User data object containing write cmd parameters
| vx_char VISSObj::output_file_path[APP_MODULES_MAX_OBJ_NAME_SIZE] |
Output file path for VISS node output
| vx_char VISSObj::obj_name[APP_MODULES_MAX_OBJ_NAME_SIZE] |
Name of VISS module