72 if (handle == NULL || bufParamsIn0 == NULL || bufParamsIn1 == NULL || bufParamsOut == NULL || pKerInitArgs == NULL) {
86 if ((bufParamsIn0->
dim_x != bufParamsIn1->
dim_x) || (bufParamsIn0->
dim_y != bufParamsIn1->
dim_y) ||
96 if ((strideIn0Elements < bufParamsIn0->dim_x) || (strideIn1Elements < bufParamsIn1->dim_x) ||
97 (strideOutElements < bufParamsOut->dim_x)) {
113 const void *restrict pIn0,
114 const void *restrict pIn1,
115 const void *restrict pOut)
120 printf(
"Enter VXLIB_normL1_exec_checkParams\n");
122 if ((handle == NULL) || (pIn0 == NULL) || (pIn1 == NULL) || (pOut == NULL)) {
158 printf(
"VXLIB_DEBUGPRINT Enter VXLIB_normL1_init\n");
162 uint32_t dTypeIn = bufParamsIn0->
data_type;
163 uint32_t dTypeOut = bufParamsOut->
data_type;
211 printf(
"VXLIB_DEBUGPRINT Enter VXLIB_normL1_exec\n");
216 status = pKerPrivArgs->
execute(handle, pIn0, pIn1, pOut);
template VXLIB_STATUS VXLIB_normL1_exec_ci< VXLIB_NORML1_TYPENAME_I16S_O16U >(VXLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut)
template VXLIB_STATUS VXLIB_normL1_init_ci< VXLIB_NORML1_DTYPE_I8S_O8U >(VXLIB_kernelHandle handle, const VXLIB_bufParams2D_t *bufParamsIn0, const VXLIB_bufParams2D_t *bufParamsIn1, const VXLIB_bufParams2D_t *bufParamsOut, const VXLIB_normL1_InitArgs *pKerInitArgs)
template VXLIB_STATUS VXLIB_normL1_init_ci< VXLIB_NORML1_DTYPE_I16S_O16U >(VXLIB_kernelHandle handle, const VXLIB_bufParams2D_t *bufParamsIn0, const VXLIB_bufParams2D_t *bufParamsIn1, const VXLIB_bufParams2D_t *bufParamsOut, const VXLIB_normL1_InitArgs *pKerInitArgs)
template VXLIB_STATUS VXLIB_normL1_exec_ci< VXLIB_NORML1_TYPENAME_I8S_O8U >(VXLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut)
template VXLIB_STATUS VXLIB_normL1_exec_cn< VXLIB_NORML1_TYPENAME_I16S_O16U >(VXLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut)
template VXLIB_STATUS VXLIB_normL1_exec_cn< VXLIB_NORML1_TYPENAME_I8S_O8U >(VXLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut)
Header file for kernel's internal use. For the kernel's interface, please see VXLIB_normL1.
#define VXLIB_NOMRL1_I8S_O8U
Macros that will be useful to check for datatype combinations.
#define VXLIB_NORML1_I16S_O16U
void * VXLIB_kernelHandle
Handle type for VXLIB operations.
VXLIB_STATUS_NAME
The enumeration of all status codes.
@ VXLIB_ERR_INVALID_DIMENSION
@ VXLIB_ERR_NOT_EQUAL_WIDTH_STRIDE
static int32_t VXLIB_sizeof(uint32_t type)
Inline function returns number of bytes per element given a type of VXLIB_data_type_e.
VXLIB_STATUS VXLIB_normL1_init_checkParams(VXLIB_kernelHandle handle, const VXLIB_bufParams2D_t *bufParamsIn0, const VXLIB_bufParams2D_t *bufParamsIn1, const VXLIB_bufParams2D_t *bufParamsOut, const VXLIB_normL1_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to VXLIB_normL1_init function....
VXLIB_STATUS VXLIB_normL1_exec(VXLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut)
This function is the main kernel compute function.
VXLIB_STATUS VXLIB_normL1_exec_checkParams(VXLIB_kernelHandle handle, const void *restrict pIn0, const void *restrict pIn1, const void *restrict pOut)
This function checks the validity of the parameters passed to VXLIB_normL1_exec function....
int32_t VXLIB_normL1_getHandleSize(VXLIB_normL1_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
VXLIB_STATUS VXLIB_normL1_init(VXLIB_kernelHandle handle, VXLIB_bufParams2D_t *bufParamsIn0, VXLIB_bufParams2D_t *bufParamsIn1, VXLIB_bufParams2D_t *bufParamsOut, const VXLIB_normL1_InitArgs *pKerInitArgs)
This function should be called before the VXLIB_normL1_exec function is called. This function takes c...
A structure for a 2 dimensional buffer descriptor.
uint32_t dim_y
Height of buffer in Y dimension in elements.
uint32_t dim_x
Width of buffer in X dimension in elements.
uint32_t data_type
Values are of type VXLIB_data_type_e.
int32_t stride_y
Stride in Y dimension in bytes.
Structure containing the parameters to initialize the kernel.
int8_t funcStyle
Variant of the function, refer to VXLIB_FUNCTION_STYLE
Structure that is reserved for internal use by the kernel.
pFxnVXLIB_normL1_exec execute
Function pointer to point to the right execution variant between VXLIB_normL1_exec_cn and VXLIB_normL...
size_t strideOutElements
Stride of output in elements.
size_t strideIn1Elements
Stride of input1 in elements.
size_t height
Height of image
size_t width
Width of image
size_t strideIn0Elements
Stride of input0 in elements.