The list of supported kernels in this kernel extension.
Go to the source code of this file.
Data Structures | |
| struct | tivx_opengl_mosaic_params_t |
| OpenGL Mosaic Node parameters. More... | |
Macros | |
| #define | TIVX_MODULE_NAME_SAMPLE "sample" |
| Name for OpenVX Extension kernel module: sample. More... | |
| #define | TIVX_KERNEL_OPENGL_MOSAIC_NAME "com.ti.sample.opengl_mosaic" |
| The list of kernels supported in sample module. More... | |
| #define | TIVX_KERNEL_OPENGL_MOSAIC_TYPE_1x1 (0) |
| The configuration data structure used by the TIVX_KERNEL_OPENGL_MOSAIC kernel. More... | |
| #define | TIVX_KERNEL_OPENGL_MOSAIC_TYPE_2x2 (1) |
Functions | |
| void | tivxSampleLoadKernels (vx_context context) |
| Used for the Application to load the sample kernels into the context. More... | |
| void | tivxSampleUnLoadKernels (vx_context context) |
| Used for the Application to unload the sample kernels from the context. More... | |
| void | tivxSamplePrintPerformance (vx_perf_t performance, uint32_t numPixels, const char *testName) |
| Used to print the performance of the kernels. More... | |