Data Fields | |
| vx_node | node |
| vx_kernel | kernel |
| vx_user_data_object | config |
| vx_user_data_object | network |
| vx_user_data_object | createParams |
| vx_object_array | in_args_arr |
| vx_object_array | out_args_arr |
| vx_object_array | trace_data_arr |
| vx_object_array | output_tensor_arr [APP_MODULE_TIDL_MAX_TENSORS] |
| vx_uint32 | num_input_tensors |
| vx_uint32 | core_id |
| vx_uint32 | num_output_tensors |
| vx_int32 | graph_parameter_index |
| vx_char | config_file_path [APP_MODULES_MAX_FILE_PATH_SIZE] |
| vx_char | network_file_path [APP_MODULES_MAX_FILE_PATH_SIZE] |
| vx_char | objName [APP_MODULES_MAX_OBJ_NAME_SIZE] |
| vx_uint8 | config_checksum [TIVX_TIDL_J7_CHECKSUM_SIZE] |
| vx_uint8 | network_checksum [TIVX_TIDL_J7_CHECKSUM_SIZE] |
| vx_node TIDLObj::node |
TIDL node object
| vx_kernel TIDLObj::kernel |
TIDL kernel object
| vx_user_data_object TIDLObj::config |
TIDL config user data object
| vx_user_data_object TIDLObj::network |
TIDL network user data object
| vx_user_data_object TIDLObj::createParams |
TIDL create params user data object
| vx_object_array TIDLObj::in_args_arr |
TIDL create params user data object
| vx_object_array TIDLObj::out_args_arr |
TIDL object array of output args
| vx_object_array TIDLObj::trace_data_arr |
TIDL object array of trace data
| vx_object_array TIDLObj::output_tensor_arr[APP_MODULE_TIDL_MAX_TENSORS] |
TIDL object array of output tensors
| vx_uint32 TIDLObj::num_input_tensors |
TIDL number of input tensors
| vx_uint32 TIDLObj::core_id |
TIDL CPU Core_ID
| vx_uint32 TIDLObj::num_output_tensors |
TIDL number of output tensors
| vx_int32 TIDLObj::graph_parameter_index |
TIDL graph parameter index
| vx_char TIDLObj::config_file_path[APP_MODULES_MAX_FILE_PATH_SIZE] |
Config structure file path
| vx_char TIDLObj::network_file_path[APP_MODULES_MAX_FILE_PATH_SIZE] |
Network structure file path
| vx_char TIDLObj::objName[APP_MODULES_MAX_OBJ_NAME_SIZE] |
Name of TIDL module
| vx_uint8 TIDLObj::config_checksum[TIVX_TIDL_J7_CHECKSUM_SIZE] |
Config structure checksum
| vx_uint8 TIDLObj::network_checksum[TIVX_TIDL_J7_CHECKSUM_SIZE] |
Network structure checksum