Vision Apps User Guide
NetworkCtrl_CmdHeader Struct Reference

Data Fields

uint32_t header
 
char cmd [NETWORK_CTRL_CMD_STRLEN_MAX]
 
uint32_t returnValue
 
uint32_t flags
 
uint32_t prmSize
 

Field Documentation

◆ header

uint32_t NetworkCtrl_CmdHeader::header

Header magic number NETWORK_CTRL_HEADER

◆ cmd

char NetworkCtrl_CmdHeader::cmd[NETWORK_CTRL_CMD_STRLEN_MAX]

Command, specified as a string of char's

◆ returnValue

uint32_t NetworkCtrl_CmdHeader::returnValue

Return value that is set by the command handler

◆ flags

uint32_t NetworkCtrl_CmdHeader::flags

command specified flags, see NETWORK_CTRL_FLAG_*

◆ prmSize

uint32_t NetworkCtrl_CmdHeader::prmSize

Size of input parameters in units of bytes. Can be 0 if no parameters need to sent for a command