Data Fields | |
| uint8_t * | addr |
| uint32_t | width |
| uint32_t | height |
| uint32_t | bpp |
| uint32_t | lineOffset |
| uint32_t | num |
| uint32_t | colorFormat |
| uint8_t* Draw2D_FontProperty::addr |
memory address location of the font
| uint32_t Draw2D_FontProperty::width |
Width of a character of font in pixels
| uint32_t Draw2D_FontProperty::height |
Height of a character of font in lines
| uint32_t Draw2D_FontProperty::bpp |
bytes per pixel of the font in bytes
| uint32_t Draw2D_FontProperty::lineOffset |
line offset of the font in bytes
| uint32_t Draw2D_FontProperty::num |
Number of characters in font
| uint32_t Draw2D_FontProperty::colorFormat |
Currently below data formats are supported