This section contains APIs to use CODEC Pipelines within demos.
◆ CODEC_MAX_LEN_CMD_STR
| #define CODEC_MAX_LEN_CMD_STR 4096u |
◆ CODEC_MAX_LEN_ELEM_NAME
| #define CODEC_MAX_LEN_ELEM_NAME 32u |
◆ CODEC_MAX_NUM_PLANES
| #define CODEC_MAX_NUM_PLANES 4u |
◆ CODEC_MAX_BUFFER_DEPTH
| #define CODEC_MAX_BUFFER_DEPTH 16u |
◆ CODEC_MAX_NUM_CHANNELS
| #define CODEC_MAX_NUM_CHANNELS 8u |
◆ appCodecInit()
Launches the CODECPipeline described by user defined parameters. Initializes the codec_wrapper and calls gst_parse_launch() on the command string.
- Parameters
-
◆ appCodecSrcInit()
| int32_t appCodecSrcInit |
( |
void * |
data_ptr[CODEC_MAX_BUFFER_DEPTH][CODEC_MAX_NUM_CHANNELS][CODEC_MAX_NUM_PLANES] | ) |
|
Initializes the AppSrc elements to be able to push buffers to the CODECPipeline. Wraps the given allocated memory as CODECBuffers to push. The input parameters (in_*) must be properly initialised.
- Parameters
-
| [in] | data_ptr | memory that the CODECBuffers will map to |
◆ appCodecSinkInit()
| int32_t appCodecSinkInit |
( |
void * |
data_ptr[CODEC_MAX_BUFFER_DEPTH][CODEC_MAX_NUM_CHANNELS][CODEC_MAX_NUM_PLANES] | ) |
|
Initializes the AppSink elements to be able to pull buffers from the CODECPipeline. Registers the data_pointers that will map to the bufferpool of pulled CODECBuffers. The output parameters (out_*) must be properly initialised.
- Parameters
-
| [in] | data_ptr | memory that the CODECBuffers will map to |
◆ appCodecStart()
| int32_t appCodecStart |
( |
| ) |
|
Starts the CODECPipeline that was launched previously.
◆ appCodecEnqAppSrc()
| int32_t appCodecEnqAppSrc |
( |
uint8_t |
idx | ) |
|
Push a buffer from the bufferpool to the AppSrc element.
- Parameters
-
| [in] | idx | the buffer id, from the bufferpool, to be pushed to the CODECPipeline |
◆ appCodecDeqAppSrc()
| int32_t appCodecDeqAppSrc |
( |
uint8_t |
idx | ) |
|
Wait for a previously pushed buffer to be consumed by the CODECPipeline.
- Parameters
-
| [in] | idx | the buffer id, from the bufferpool, to wait on |
◆ appCodecEnqEosAppSrc()
| int32_t appCodecEnqEosAppSrc |
( |
| ) |
|
Push EOS (End Of Stream) to the AppSrc element. Signals the elements to stop processing buffers after this.
◆ appCodecDeqAppSink()
| int32_t appCodecDeqAppSink |
( |
uint8_t |
idx | ) |
|
Pull a buffer from the AppSink element into the bufferpool.
- Parameters
-
| [in] | idx | the slot into which the pulled data is stored in the pulled_data_ptr array, while maintaining a reference to the pulled CODECBuffer |
◆ appCodecEnqAppSink()
| int32_t appCodecEnqAppSink |
( |
uint8_t |
idx | ) |
|
Release a previously pulled CODECBuffer back to GStreamer and cleanup.
- Parameters
-
| [in] | idx | the slot from which the buffer is released back to CODECreamer. The data pointer for this slot is no longer valid |
◆ appCodecStop()
Stops the CODECPipeline that was in playing state. If there is no AppSink element, waits to recieve EOS before cleaning up.
◆ appCodecDeInit()
Unmaps all buffers that were mapped and destroys all GStreamer or OpenMAX objects.
◆ appCodecPrintStats()
| void appCodecPrintStats |
( |
| ) |
|
Prints the current count of the numbers of buffers pushed/pulled to/from the CODECPipeline. Not multi-thread safe.