![]() |
TIOVX User Guide
|
This data structure is used to return information about kernel parameters via the vxGetKernelParameterConfig API. More...
#include <vx_khr_pipelining.h>
Data Fields | |
| vx_uint32 | index |
| index of the parameter, starting at zero | |
| vx_enum | type |
| an object type, such as VX_TYPE_IMAGE | |
| vx_enum | direction |
| VX_INPUT, VX_OUTPUT or VX_BIDIRECTIONAL. | |
| vx_enum | state |
| X_PARAMETER_STATE_REQUIRED or VX_PARAMETER_STATE_OPTIONAL. | |
| vx_meta_format | meta |
| More information about the parameter, if not NULL, this will need releasing. | |
This data structure is used to return information about kernel parameters via the vxGetKernelParameterConfig API.
Definition at line 977 of file vx_khr_pipelining.h.