![]() |
TIOVX User Guide
|
Internal APIs for platform operations.
Data Structures | |
| struct | tivx_shm_obj_count_t |
| Struct containing object descriptor allocation counts. Allows for a log to be kept of the object descriptors used throughout runtime. More... | |
Defines | |
| #define | TIVX_PLATFORM_SHM_ENTRY_SIZE_ALIGN (8U) |
| Macro to check the alignment of the size of the shared memory entry. | |
| #define | TIVX_PLATFORM_LOCK_LOG_RT_HW_SPIN_LOCK_ID (253u) |
| HW spinlock ID to use for locking run-time event logger. | |
| #define | TIVX_PLATFORM_LOCK_OBJ_DESC_TABLE_HW_SPIN_LOCK_ID (254u) |
| HW spinlock ID to use for locking object descriptor table. | |
| #define | TIVX_PLATFORM_LOCK_DATA_REF_QUEUE_HW_SPIN_LOCK_ID (255u) |
| HW spinlock ID to use for locking data ref queue. | |
| #define | TIVX_TARGET_R5F_MAX (27U) |
| Max number of targets on a given R5F. | |
| #define | TIVX_TARGET_INFO |
| Mapping of Target names with Target Ids Used to initialize internal structure. | |
| #define | ASSERT_CONCAT_(a, b) a##b |
| Macros for build time check. | |
| #define | TIVX_PLATFORM_MAX_OBJ_DESC_SHM_INST (4096u) |
| Maximum number obj descriptors that are present in shared memory. | |
Enumerations | |
| enum | tivx_platform_lock_type_e { TIVX_PLATFORM_LOCK_OBJ_DESC_TABLE = 0, TIVX_PLATFORM_LOCK_CONTEXT, TIVX_PLATFORM_LOCK_DATA_REF_QUEUE, TIVX_PLATFORM_LOCK_LOG_RT_INDEX, TIVX_PLATFORM_LOCK_LOG_RT, TIVX_PLATFORM_LOCK_MAX } |
| Types of system level locks. More... | |
| enum | tivx_target_id_e { TIVX_TARGET_ID_DSP_C7_1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_1, 0u), TIVX_TARGET_ID_DSP_C7_1_PRI_2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_1, 1u), TIVX_TARGET_ID_DSP_C7_1_PRI_3 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_1, 2u), TIVX_TARGET_ID_DSP_C7_1_PRI_4 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_1, 3u), TIVX_TARGET_ID_DSP_C7_1_PRI_5 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_1, 4u), TIVX_TARGET_ID_DSP_C7_1_PRI_6 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_1, 5u), TIVX_TARGET_ID_DSP_C7_1_PRI_7 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_1, 6u), TIVX_TARGET_ID_DSP_C7_1_PRI_8 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_1, 7u), TIVX_TARGET_ID_DSP_C7_2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_2, 0u), TIVX_TARGET_ID_DSP_C7_2_PRI_2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_2, 1u), TIVX_TARGET_ID_DSP_C7_2_PRI_3 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_2, 2u), TIVX_TARGET_ID_DSP_C7_2_PRI_4 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_2, 3u), TIVX_TARGET_ID_DSP_C7_2_PRI_5 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_2, 4u), TIVX_TARGET_ID_DSP_C7_2_PRI_6 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_2, 5u), TIVX_TARGET_ID_DSP_C7_2_PRI_7 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_2, 6u), TIVX_TARGET_ID_DSP_C7_2_PRI_8 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_2, 7u), TIVX_TARGET_ID_DSP_C7_3 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_3, 0u), TIVX_TARGET_ID_DSP_C7_3_PRI_2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_3, 1u), TIVX_TARGET_ID_DSP_C7_3_PRI_3 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_3, 2u), TIVX_TARGET_ID_DSP_C7_3_PRI_4 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_3, 3u), TIVX_TARGET_ID_DSP_C7_3_PRI_5 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_3, 4u), TIVX_TARGET_ID_DSP_C7_3_PRI_6 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_3, 5u), TIVX_TARGET_ID_DSP_C7_3_PRI_7 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_3, 6u), TIVX_TARGET_ID_DSP_C7_3_PRI_8 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_DSP_C7_3, 7u), TIVX_TARGET_ID_MPU_0 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MPU_0, 0u), TIVX_TARGET_ID_MPU_1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MPU_0, 1u), TIVX_TARGET_ID_MPU_2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MPU_0, 2u), TIVX_TARGET_ID_MPU_3 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MPU_0, 3u), TIVX_TARGET_ID_MCU2_0 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 0u), TIVX_TARGET_ID_VPAC_NF = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 1u), TIVX_TARGET_ID_VPAC_LDC1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 2u), TIVX_TARGET_ID_VPAC_MSC1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 3u), TIVX_TARGET_ID_VPAC_MSC2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 4u), TIVX_TARGET_ID_VPAC_VISS1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 5u), TIVX_TARGET_ID_CAPTURE1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 6u), TIVX_TARGET_ID_CAPTURE2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 7u), TIVX_TARGET_ID_DISPLAY1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 8u), TIVX_TARGET_ID_DISPLAY2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 9u), TIVX_TARGET_ID_CSITX = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 10u), TIVX_TARGET_ID_CAPTURE3 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 11u), TIVX_TARGET_ID_CAPTURE4 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 12u), TIVX_TARGET_ID_CAPTURE5 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 13u), TIVX_TARGET_ID_CAPTURE6 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 14u), TIVX_TARGET_ID_CAPTURE7 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 15u), TIVX_TARGET_ID_CAPTURE8 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 16u), TIVX_TARGET_ID_CAPTURE9 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 17u), TIVX_TARGET_ID_CAPTURE10 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 18u), TIVX_TARGET_ID_CAPTURE11 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 19u), TIVX_TARGET_ID_CAPTURE12 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 20u), TIVX_TARGET_ID_DISPLAY_M2M1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 21u), TIVX_TARGET_ID_DISPLAY_M2M2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 22u), TIVX_TARGET_ID_DISPLAY_M2M3 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 23u), TIVX_TARGET_ID_DISPLAY_M2M4 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 24u), TIVX_TARGET_ID_CSITX2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 25u), TIVX_TARGET_ID_VPAC_FC = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_0, 26u), TIVX_TARGET_ID_MCU2_1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_1, 0u), TIVX_TARGET_ID_DMPAC_SDE = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_1, 1u), TIVX_TARGET_ID_DMPAC_DOF = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU2_1, 2u), TIVX_TARGET_ID_MCU3_0 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU3_0, 0u), TIVX_TARGET_ID_MCU3_1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU3_1, 0u), TIVX_TARGET_ID_MCU4_0 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU4_0, 0u), TIVX_TARGET_ID_VPAC2_NF = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU4_0, 1u), TIVX_TARGET_ID_VPAC2_LDC1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU4_0, 2u), TIVX_TARGET_ID_VPAC2_MSC1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU4_0, 3u), TIVX_TARGET_ID_VPAC2_MSC2 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU4_0, 4u), TIVX_TARGET_ID_VPAC2_VISS1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU4_0, 5u), TIVX_TARGET_ID_VPAC2_FC = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU4_0, 6u), TIVX_TARGET_ID_MCU4_1 = TIVX_MAKE_TARGET_ID(TIVX_CPU_ID_MCU4_1, 0u) } |
| Target ID for supported targets. More... | |
Functions | |
| vx_status | ownMemBufferMap (void *host_ptr, uint32_t size, vx_enum mem_type, vx_enum maptype) |
| Internal-only buffer map function used to selectively apply cache maintenance operations based on the underlying OS implementation. | |
| vx_status | ownMemBufferUnmap (void *host_ptr, uint32_t size, vx_enum mem_type, vx_enum maptype) |
| Internal-only buffer unmap function used to selectively apply cache maintenance operations based on the underlying OS implementation. | |
| int32_t | tivxPlatformGetShmSize (uint32_t *shm_size) |
| Get size of TIOVX object descriptor memory carveout. More... | |
| void | ownTableIncrementValue (vx_enum resource_name) |
| Increment count of given resource. More... | |
| void | ownTableDecrementValue (vx_enum resource_name) |
| Decrement count of given resource. More... | |
| vx_enum | ownPlatformGetTargetId (const char *target_name) |
| Convert a target name to a specific target ID. More... | |
| void | ownPlatformGetTargetName (vx_enum target_id, char *target_name) |
| Convert a specific target ID to a target name. More... | |
| void | ownPlatformGetObjDescTableInfo (tivx_obj_desc_table_info_t *table_info) |
| Return shared memory info which holds the object descriptors. More... | |
| void | ownPlatformGetLogRtShmInfo (void **shm_base, uint32_t *shm_size) |
| Return shared memory info which holds the run-time logger buffer. More... | |
| void | ownPlatformSystemLock (vx_enum lock_id) |
| Take a system level lock. More... | |
| void | ownPlatformSystemUnlock (vx_enum lock_id) |
| Release system level lock. | |
| vx_status | ownPlatformInit (void) |
| Init Platform module. | |
| void | ownPlatformDeInit (void) |
| DeInit Platform module. | |
| void | ownPlatformPrintf (const char *format) |
| Print given string. | |
| void | ownPlatformCreateTargets (void) |
| Function to set the target configuration. More... | |
| void | ownPlatformDeleteTargets (void) |
| Function to destroy created targets. | |
| void | ownPlatformActivate (void) |
| Utility function to enable Platform specific things Currently Used for EVE algorithm to enable EDMA. | |
| void | ownPlatformDeactivate (void) |
| Utility function to disable Platform specific things Currently Used for EVE algorithm to disable EDMA. | |
| void | ownPlatformTaskInit (void) |
| Utility function to call OS-specific task init functions. | |
| void | ownPlatformGetTargetPerfStats (uint32_t app_cpu_id, uint32_t target_values[TIVX_TARGET_RESOURCE_COUNT]) |
| Function to query targets for their TIOVX resource statistics. | |
| void | tivxPlatformCreateTargetId (vx_enum target_id, uint32_t i, const char *name, uint32_t task_pri) |
| Create target ID. | |
| void | tivxPlatformDeleteTargetId (vx_enum target_id) |
| Delete target ID. | |
| void | tivxPlatformSetHostTargetId (tivx_target_id_e host_target_id) |
| Set target ID for HOST. More... | |
Types of system level locks.
Definition at line 86 of file tivx_platform.h.
| enum tivx_target_id_e |
Target ID for supported targets.
Must be in order of consecutive index numbers per CPU ID. If some targets are moved to a different CPU, the order and indexing should be updated accordingly.
Definition at line 89 of file tivx_target_config_j742s2.h.
| int32_t tivxPlatformGetShmSize | ( | uint32_t * | shm_size | ) |
Get size of TIOVX object descriptor memory carveout.
| shm_size | [in] Address of unsigned int to hold size of shared memory |
| void ownTableIncrementValue | ( | vx_enum | resource_name | ) |
Increment count of given resource.
| resource_name | [in] Enum of resource whose count should be updated |
| void ownTableDecrementValue | ( | vx_enum | resource_name | ) |
Decrement count of given resource.
| resource_name | [in] Enum of resource whose count should be updated |
| vx_enum ownPlatformGetTargetId | ( | const char * | target_name | ) |
Convert a target name to a specific target ID.
| target_name | [in] Target name |
| void ownPlatformGetTargetName | ( | vx_enum | target_id, |
| char * | target_name | ||
| ) |
Convert a specific target ID to a target name.
| target_id | [in] Target ID |
| target_name | [out] Target name |
| void ownPlatformGetObjDescTableInfo | ( | tivx_obj_desc_table_info_t * | table_info | ) |
Return shared memory info which holds the object descriptors.
This is platform APIs since method of specifying shared memory, number of object descriptors is platform dependant
| void ownPlatformGetLogRtShmInfo | ( | void ** | shm_base, |
| uint32_t * | shm_size | ||
| ) |
Return shared memory info which holds the run-time logger buffer.
This is platform APIs since method of specifying shared memory, is platform dependant
| void ownPlatformSystemLock | ( | vx_enum | lock_id | ) |
Take a system level lock.
This locks is taken across all targets to mutual exclusion across targets
WARNING: No OS calls shall be made after calling this function until the ownPlatformSystemUnlock has been called due to the chance that interrupts may be disabled during this duration.
| void ownPlatformCreateTargets | ( | void | ) |
Function to set the target configuration.
It creates target and adds it to the list of targets supported on each core.
| void tivxPlatformSetHostTargetId | ( | tivx_target_id_e | host_target_id | ) |
Set target ID for HOST.
Called during tivxHostInit()