![]() |
TIOVX User Guide
|
TI Targets (for vxSetNodeTarget)
The following list of defines are the list of targets supported for the call to vxSetNodeTarget
Defines | |
| #define | TIVX_TARGET_MPU_0 "MPU-0" |
| Target name for MPU_0. | |
| #define | TIVX_TARGET_MPU_1 "MPU-1" |
| Target name for MPU_1. | |
| #define | TIVX_TARGET_MPU_2 "MPU-2" |
| Target name for MPU_2. | |
| #define | TIVX_TARGET_MPU_3 "MPU-3" |
| Target name for MPU_3. | |
| #define | TIVX_TARGET_DSP_C7_1 "DSP_C7-1" |
| Target name for DSP_C7_1 This target task is first in priority. Each of the C7X targets are assigned a different task priority. Subsequent C7X targets are assigned lower priority than the preceding target (i.e., TIVX_TARGET_DSP_C7_1_PRI_2 is lower priority than TIVX_TARGET_DSP_C7_1_PRI_1). Therefore, the TIVX_TARGET_DSP_C7_1_PRI_2 target will be preempted by TIVX_TARGET_DSP_C7_1_PRI_1 once the higher priority target is unblocked to execute. | |
| #define | TIVX_TARGET_DSP_C7_1_PRI_1 TIVX_TARGET_DSP_C7_1 |
| Target name for DSP_C7_1 This target task is first in priority. This aliases to the same task as TIVX_TARGET_DSP_C7_1. | |
| #define | TIVX_TARGET_DSP_C7_1_PRI_2 "DSP_C7-1_PRI_2" |
| Target name for DSP_C7-1_PRI_2 This target task is second in priority. | |
| #define | TIVX_TARGET_DSP_C7_1_PRI_3 "DSP_C7-1_PRI_3" |
| Target name for DSP_C7-1_PRI_3 This target task is third in priority. | |
| #define | TIVX_TARGET_DSP_C7_1_PRI_4 "DSP_C7-1_PRI_4" |
| Target name for DSP_C7-1_PRI_4 This target task is fourth in priority. | |
| #define | TIVX_TARGET_DSP_C7_1_PRI_5 "DSP_C7-1_PRI_5" |
| Target name for DSP_C7-1_PRI_5 This target task is fifth in priority. | |
| #define | TIVX_TARGET_DSP_C7_1_PRI_6 "DSP_C7-1_PRI_6" |
| Target name for DSP_C7-1_PRI_6 This target task is sixth in priority. | |
| #define | TIVX_TARGET_DSP_C7_1_PRI_7 "DSP_C7-1_PRI_7" |
| Target name for DSP_C7-1_PRI_7 This target task is seventh in priority. | |
| #define | TIVX_TARGET_DSP_C7_1_PRI_8 "DSP_C7-1_PRI_8" |
| Target name for DSP_C7-1_PRI_8 This target task is eighth in priority. | |
| #define | TIVX_TARGET_DSP_C7_2 "DSP_C7-2" |
| Target name for DSP_C7_2 This target task is first in priority. Each of the C7X targets are assigned a different task priority. Subsequent C7X targets are assigned lower priority than the preceding target (i.e., TIVX_TARGET_DSP_C7_2_PRI_2 is lower priority than TIVX_TARGET_DSP_C7_2_PRI_1). Therefore, the TIVX_TARGET_DSP_C7_2_PRI_2 target will be preempted by TIVX_TARGET_DSP_C7_2_PRI_1 once the higher priority target is unblocked to execute. | |
| #define | TIVX_TARGET_DSP_C7_2_PRI_1 TIVX_TARGET_DSP_C7_2 |
| Target name for DSP_C7_2 This target task is first in priority. This aliases to the same task as TIVX_TARGET_DSP_C7_2. | |
| #define | TIVX_TARGET_DSP_C7_2_PRI_2 "DSP_C7-2_PRI_2" |
| Target name for DSP_C7-2_PRI_2 This target task is second in priority. | |
| #define | TIVX_TARGET_DSP_C7_2_PRI_3 "DSP_C7-2_PRI_3" |
| Target name for DSP_C7-2_PRI_3 This target task is third in priority. | |
| #define | TIVX_TARGET_DSP_C7_2_PRI_4 "DSP_C7-2_PRI_4" |
| Target name for DSP_C7-2_PRI_4 This target task is fourth in priority. | |
| #define | TIVX_TARGET_DSP_C7_2_PRI_5 "DSP_C7-2_PRI_5" |
| Target name for DSP_C7-2_PRI_5 This target task is fifth in priority. | |
| #define | TIVX_TARGET_DSP_C7_2_PRI_6 "DSP_C7-2_PRI_6" |
| Target name for DSP_C7-2_PRI_6 This target task is sixth in priority. | |
| #define | TIVX_TARGET_DSP_C7_2_PRI_7 "DSP_C7-2_PRI_7" |
| Target name for DSP_C7-2_PRI_7 This target task is seventh in priority. | |
| #define | TIVX_TARGET_DSP_C7_2_PRI_8 "DSP_C7-2_PRI_8" |
| Target name for DSP_C7-2_PRI_8 This target task is eighth in priority. | |
| #define | TIVX_TARGET_DSP_C7_3 "DSP_C7-3" |
| Target name for DSP_C7_3 This target task is first in priority. Each of the C7X targets are assigned a different task priority. Subsequent C7X targets are assigned lower priority than the preceding target (i.e., TIVX_TARGET_DSP_C7_3_PRI_2 is lower priority than TIVX_TARGET_DSP_C7_3_PRI_1). Therefore, the TIVX_TARGET_DSP_C7_3_PRI_2 target will be preempted by TIVX_TARGET_DSP_C7_3_PRI_1 once the higher priority target is unblocked to execute. | |
| #define | TIVX_TARGET_DSP_C7_3_PRI_1 TIVX_TARGET_DSP_C7_3 |
| Target name for DSP_C7_3 This target task is first in priority. This aliases to the same task as TIVX_TARGET_DSP_C7_3. | |
| #define | TIVX_TARGET_DSP_C7_3_PRI_2 "DSP_C7-3_PRI_2" |
| Target name for DSP_C7-3_PRI_2 This target task is second in priority. | |
| #define | TIVX_TARGET_DSP_C7_3_PRI_3 "DSP_C7-3_PRI_3" |
| Target name for DSP_C7-3_PRI_3 This target task is third in priority. | |
| #define | TIVX_TARGET_DSP_C7_3_PRI_4 "DSP_C7-3_PRI_4" |
| Target name for DSP_C7-3_PRI_4 This target task is fourth in priority. | |
| #define | TIVX_TARGET_DSP_C7_3_PRI_5 "DSP_C7-3_PRI_5" |
| Target name for DSP_C7-3_PRI_5 This target task is fifth in priority. | |
| #define | TIVX_TARGET_DSP_C7_3_PRI_6 "DSP_C7-3_PRI_6" |
| Target name for DSP_C7-3_PRI_6 This target task is sixth in priority. | |
| #define | TIVX_TARGET_DSP_C7_3_PRI_7 "DSP_C7-3_PRI_7" |
| Target name for DSP_C7-3_PRI_7 This target task is seventh in priority. | |
| #define | TIVX_TARGET_DSP_C7_3_PRI_8 "DSP_C7-3_PRI_8" |
| Target name for DSP_C7-3_PRI_8 This target task is eighth in priority. | |
| #define | TIVX_TARGET_DSP1 TIVX_TARGET_DSP_C7_2 |
| Name for DSP target class, instance 1. More... | |
| #define | TIVX_TARGET_MCU2_0 "MCU2-0" |
| Name for MCU2 target class, core 0. More... | |
| #define | TIVX_TARGET_MCU2_1 "MCU2-1" |
| Name for MCU2 target class, core 1. More... | |
| #define | TIVX_TARGET_MCU3_0 "MCU3-0" |
| Name for MCU3_0 target class, core 0. More... | |
| #define | TIVX_TARGET_MCU3_1 "MCU3-1" |
| Name for MCU3_1 target class, core 1. More... | |
| #define | TIVX_TARGET_MCU4_0 "MCU4-0" |
| Name for MCU4_0 target class, core 0. More... | |
| #define | TIVX_TARGET_MCU4_1 "MCU4-1" |
| Name for MCU4_1 target class, core 1. More... | |
| #define | TIVX_TARGET_CAPTURE1 "CAPTURE1" |
| Target name for Capture. | |
| #define | TIVX_TARGET_CAPTURE2 "CAPTURE2" |
| Target name for Capture. | |
| #define | TIVX_TARGET_CAPTURE3 "CAPTURE3" |
| Target name for Capture Node Instance 3. | |
| #define | TIVX_TARGET_CAPTURE4 "CAPTURE4" |
| Target name for Capture Node Instance 4. | |
| #define | TIVX_TARGET_CAPTURE5 "CAPTURE5" |
| Target name for Capture Node Instance 5. | |
| #define | TIVX_TARGET_CAPTURE6 "CAPTURE6" |
| Target name for Capture Node Instance 6. | |
| #define | TIVX_TARGET_CAPTURE7 "CAPTURE7" |
| Target name for Capture Node Instance 7. | |
| #define | TIVX_TARGET_CAPTURE8 "CAPTURE8" |
| Target name for Capture Node Instance 8. | |
| #define | TIVX_TARGET_CAPTURE9 "CAPTURE9" |
| Target name for Capture Node Instance 9. | |
| #define | TIVX_TARGET_CAPTURE10 "CAPTURE10" |
| Target name for Capture Node Instance 10. | |
| #define | TIVX_TARGET_CAPTURE11 "CAPTURE11" |
| Target name for Capture Node Instance 11. | |
| #define | TIVX_TARGET_CAPTURE12 "CAPTURE12" |
| Target name for Capture Node Instance 12. | |
| #define | TIVX_TARGET_CSITX "CSITX" |
| Target name for CSITX. | |
| #define | TIVX_TARGET_CSITX2 "CSITX2" |
| Target name for CSITX2. | |
| #define | TIVX_TARGET_DISPLAY_M2M1 "DSS_M2M1" |
| Target name for Display M2M Node Instance 1. | |
| #define | TIVX_TARGET_DISPLAY_M2M2 "DSS_M2M2" |
| Target name for Display M2M Node Instance 2. | |
| #define | TIVX_TARGET_DISPLAY_M2M3 "DSS_M2M3" |
| Target name for Display M2M Node Instance 3. | |
| #define | TIVX_TARGET_DISPLAY_M2M4 "DSS_M2M4" |
| Target name for Display M2M Node Instance 4. | |
| #define | TIVX_TARGET_DISPLAY1 "DISPLAY1" |
| Target name for Display. | |
| #define | TIVX_TARGET_DISPLAY2 "DISPLAY2" |
| Target name for Display. | |
| #define | TIVX_TARGET_DMPAC_DOF "DMPAC_DOF" |
| Target name for DMPAC DOF. | |
| #define | TIVX_TARGET_DMPAC_SDE "DMPAC_SDE" |
| Target name for DMPAC SDE. | |
| #define | TIVX_TARGET_VPAC1_LDC1 "VPAC_LDC1" |
| Target name for VPAC1 LDC1. | |
| #define | TIVX_TARGET_VPAC2_LDC1 "VPAC2_LDC1" |
| Target name for VPAC2 LDC1. | |
| #define | TIVX_TARGET_VPAC1_MSC1 "VPAC_MSC1" |
| Target name for VPAC1 MSC1. | |
| #define | TIVX_TARGET_VPAC1_MSC2 "VPAC_MSC2" |
| Target name for VPAC1 MSC2. | |
| #define | TIVX_TARGET_VPAC2_MSC1 "VPAC2_MSC1" |
| Target name for VPAC2 MSC1. | |
| #define | TIVX_TARGET_VPAC2_MSC2 "VPAC2_MSC2" |
| Target name for VPAC2 MSC2. | |
| #define | TIVX_TARGET_VPAC1_NF "VPAC_NF" |
| Target name for VPAC1 NF. | |
| #define | TIVX_TARGET_VPAC2_NF "VPAC2_NF" |
| Target name for VPAC2 NF. | |
| #define | TIVX_TARGET_VPAC1_VISS1 "VPAC_VISS1" |
| Target name for VPAC1 VISS1. | |
| #define | TIVX_TARGET_VPAC2_VISS1 "VPAC2_VISS1" |
| Target name for VPAC2 VISS1. | |
| #define | TIVX_TARGET_VPAC1_FC "VPAC1_FC" |
| Target name for VPAC1 FC. | |
| #define | TIVX_TARGET_VPAC2_FC "VPAC2_FC" |
| Target name for VPAC2 FC. | |
| #define TIVX_TARGET_DSP1 TIVX_TARGET_DSP_C7_2 |
Name for DSP target class, instance 1.
Assigned to DSP_C7_2 core
Definition at line 298 of file tivx_soc_j742s2.h.
| #define TIVX_TARGET_MCU2_0 "MCU2-0" |
Name for MCU2 target class, core 0.
Assigned to MCU2_0 core
Definition at line 306 of file tivx_soc_j742s2.h.
| #define TIVX_TARGET_MCU2_1 "MCU2-1" |
Name for MCU2 target class, core 1.
Assigned to MCU2_1 core
Definition at line 314 of file tivx_soc_j742s2.h.
| #define TIVX_TARGET_MCU3_0 "MCU3-0" |
Name for MCU3_0 target class, core 0.
Assigned to MCU3_0 core
Definition at line 322 of file tivx_soc_j742s2.h.
| #define TIVX_TARGET_MCU3_1 "MCU3-1" |
Name for MCU3_1 target class, core 1.
Assigned to MCU3_1 core
Definition at line 330 of file tivx_soc_j742s2.h.
| #define TIVX_TARGET_MCU4_0 "MCU4-0" |
Name for MCU4_0 target class, core 0.
Assigned to MCU4_0 core
Definition at line 338 of file tivx_soc_j742s2.h.
| #define TIVX_TARGET_MCU4_1 "MCU4-1" |
Name for MCU4_1 target class, core 1.
Assigned to MCU4_1 core
Definition at line 346 of file tivx_soc_j742s2.h.