MCUSW
MCAL Memory Statistics

Introduction

The following tables list the memory consumed by MCAL drivers and their example application. These tables are generated from the static analysis of MCAL drivers and example implementation.


Memory Statistics for J721e

Memstats for j721e (release)

Module Code Size (Bytes) Data (Bytes) Un Initialized Data (Bytes)*
EthTrcv 2474 3 82
CddIpc 1510 4 11940
Dio 1124 160 0
Adc 3632 4 852
Pwm 3620 121 1352
Gpt 4262 132 392
Eth 15094 9383 667944
Fls 10172 656 24
Wdg 886 49 44
Spi 5426 45 1500
Can 8630 65 23052

*Please note that the un-initialized segment includes the memory consumed by the MCAL example application.

Back To Top


Memory Statistics for J7200

Memstats for j7200 (release)

Module Code Size (Bytes) Data (Bytes) Un Initialized Data (Bytes)*
EthTrcv 2474 3 82
CddIpc 1498 4 6820
Dio 1140 96 0
Adc 3584 4 448
Pwm 3620 121 1352
Gpt 4262 132 392
Eth 15102 9383 667664
Fls 10486 656 24
Wdg 886 25 44
Spi 5426 45 1500
Can 8630 65 23068
Mcu 648 13 9

*Please note that the un-initialized segment includes the memory consumed by the MCAL example application.