The flash driver provides services for reading, writing and erasing flash memory.
The Flash Driver implements a standardized interface specified in the AUTOSAR_SWS_FlashDriver document.
Only the following combinations of modes are supported:
- Direct Access Mode, Double Transfer Rate
- Direct Access Mode, Single Transfer Rate
- Indirect Access Mode, Double Tranfer Rate
- Indirect Access Mode, Single Transfer Rate
- Direct Access Mode, Poll Mode
- Indirect Access Mode, Poll Mode
- Indirect Access Mode, Interrupt Mode
- Direct Access Mode, XIP mode
Following combinations of modes are not supported:
- Direct Access Mode with Interrupt Mode, Cancel API
- See also
- FLS Configuration
|
| void | Fls_SwitchMode (boolean dacEnable, boolean xipEnable) |
| | Switch Mode of the OSPI Driver Parameters (in) : boolean dacEnable - should DAC mode be enaled or disabled Parameters (in) : boolean xipEnable - should XIP mode be enaled or disabled Mode : Supervisor Mode (Privileged Mode) More...
|
| |
| void | Fls_Init (const Fls_ConfigType *ConfigPtr) |
| | Initializes the Flash Driver. More...
|
| |
| Std_ReturnType | Fls_Erase (Fls_AddressType TargetAddress, Fls_LengthType Length) |
| | Erases flash sector(s). More...
|
| |
| Std_ReturnType | Fls_Write (Fls_AddressType TargetAddress, const uint8 *SourceAddressPtr, Fls_LengthType Length) |
| | Writes one or more complete flash pages. More...
|
| |
| Std_ReturnType | Fls_Read (Fls_AddressType SourceAddress, uint8 *TargetAddressPtr, Fls_LengthType Length) |
| | Reads from flash memory.. More...
|
| |
| Std_ReturnType | Fls_Compare (Fls_AddressType SourceAddress, const uint8 *TargetAddressPtr, Fls_LengthType Length) |
| | Compares the contents of an area of flash memory with that of an application data buffer. More...
|
| |
| Std_ReturnType | Fls_BlankCheck (Fls_AddressType Address, Fls_LengthType Length) |
| | The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed. More...
|
| |
| MemIf_StatusType | Fls_GetStatus (void) |
| | Returns the driver state. More...
|
| |
| Std_ReturnType | Fls_GetVersionInfo (Std_VersionInfoType *versioninfo) |
| | This service returns the version information of this module. More...
|
| |
| MemIf_JobResultType | Fls_GetJobResult (void) |
| | Returns the result of the last job. More...
|
| |
| void | Fls_MainFunction (void) |
| | Performs the processing of jobs. More...
|
| |
| void | Fls_Cancel (void) |
| | Cancels an ongoing job. More...
|
| |
◆ FLS_SW_MAJOR_VERSION
| #define FLS_SW_MAJOR_VERSION (11U) |
Driver Implementation Major Version.
◆ FLS_SW_MINOR_VERSION
| #define FLS_SW_MINOR_VERSION (1U) |
Driver Implementation Minor Version.
◆ FLS_SW_PATCH_VERSION
| #define FLS_SW_PATCH_VERSION (0U) |
Driver Implementation Patch Version.
◆ FLS_AR_RELEASE_MAJOR_VERSION
| #define FLS_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major version specification implemented by FLS Driver.
◆ FLS_AR_RELEASE_MINOR_VERSION
| #define FLS_AR_RELEASE_MINOR_VERSION (3U) |
AUTOSAR Minor version specification implemented by FLS Driver.
◆ FLS_AR_RELEASE_REVISION_VERSION
| #define FLS_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR Patch version specification implemented by FLS Driver.
◆ FLS_VENDOR_ID
| #define FLS_VENDOR_ID ((uint16) 44U) |
Texas Instruments Vendor ID.
◆ FLS_MODULE_ID
| #define FLS_MODULE_ID ((uint16) 92U) |
◆ FLS_INSTANCE_ID
| #define FLS_INSTANCE_ID ((uint8) 0U) |
◆ FLS_E_PARAM_CONFIG
| #define FLS_E_PARAM_CONFIG ((uint8) 0x01U) |
API service called with wrong parameter.
◆ FLS_E_PARAM_ADDRESS
| #define FLS_E_PARAM_ADDRESS ((uint8) 0x02U) |
API service called with wrong parameter.
◆ FLS_E_PARAM_LENGTH
| #define FLS_E_PARAM_LENGTH ((uint8) 0x03U) |
API service called with wrong parameter.
◆ FLS_E_PARAM_DATA
| #define FLS_E_PARAM_DATA ((uint8) 0x04U) |
API service called with wrong parameter.
◆ FLS_E_UNINIT
| #define FLS_E_UNINIT ((uint8) 0x05U) |
API service used without module initiali-zation.
◆ FLS_E_BUSY
| #define FLS_E_BUSY ((uint8) 0x06U) |
APIs called when module is busy.
◆ FLS_E_PARAM_POINTER
| #define FLS_E_PARAM_POINTER ((uint8) 0x0AU) |
APIs called with a Null Pointer.
◆ FLS_E_VERIFY_ERASE_FAILED
| #define FLS_E_VERIFY_ERASE_FAILED ((uint8) 0x07U) |
APIs service Erase Verification (BlankCheck) failed.
◆ FLS_E_VERIFY_WRITE_FAILED
| #define FLS_E_VERIFY_WRITE_FAILED ((uint8) 0x08U) |
APIs serice Write Verification (Compare) failed.
◆ FLS_E_TIMEOUT
| #define FLS_E_TIMEOUT ((uint8) 0x09U) |
◆ FLS_E_ERASE_FAILED
| #define FLS_E_ERASE_FAILED ((uint8) 0x01U) |
Flash Erase Failed in HW.
◆ FLS_E_WRITE_FAILED
| #define FLS_E_WRITE_FAILED ((uint8) 0x02U) |
Flash Write Failed in HW.
◆ FLS_E_READ_FAILED
| #define FLS_E_READ_FAILED ((uint8) 0x03U) |
◆ FLS_E_COMPARE_FAILED
| #define FLS_E_COMPARE_FAILED ((uint8) 0x04U) |
Flash Compare Failediin HW.
◆ FLS_E_UNEXPECTED_FLASH_ID
| #define FLS_E_UNEXPECTED_FLASH_ID ((uint8) 0x05U) |
Expected HW ID not matched.
◆ FLS_SID_INIT
| #define FLS_SID_INIT ((uint8) 0x00U) |
FLS_Init() API Service ID.
◆ FLS_SID_ERASE
| #define FLS_SID_ERASE ((uint8) 0x01U) |
FLS_Erase() API Service ID.
◆ FLS_SID_WRITE
| #define FLS_SID_WRITE ((uint8) 0x02U) |
FLS_Write() API Service ID.
◆ FLS_SID_CANCEL
| #define FLS_SID_CANCEL ((uint8) 0x03U) |
FLS_Cancel() API Service ID.
◆ FLS_SID_GET_STATUS
| #define FLS_SID_GET_STATUS ((uint8) 0x04U) |
FLS_GetStatus() API Service ID.
◆ FLS_SID_GET_JOB_RESULT
| #define FLS_SID_GET_JOB_RESULT ((uint8) 0x05U) |
◆ FLS_SID_READ
| #define FLS_SID_READ ((uint8) 0x07U) |
FLS_Read() API Service ID.
◆ FLS_SID_COMPARE
| #define FLS_SID_COMPARE ((uint8) 0x08U) |
FLS_Compare() API Service ID.
◆ FLS_SID_SET_MODE
| #define FLS_SID_SET_MODE ((uint8) 0x09U) |
FLS_SetMode() API Service ID.
◆ FLS_SID_GET_VERSION_INFO
| #define FLS_SID_GET_VERSION_INFO ((uint8) 0x10U) |
◆ FLS_SID_BLANK_CHECK
| #define FLS_SID_BLANK_CHECK ((uint8) 0x0AU) |
FLS_BlankCheck() API Service ID.
◆ FLS_SID_MAIN_FUNCTION
| #define FLS_SID_MAIN_FUNCTION ((uint8) 0x06U) |
FLS_MainFunction() API Service ID.
◆ Fls_AddressType
◆ Fls_LengthType
◆ Fls_SwitchMode()
| void Fls_SwitchMode |
( |
boolean |
dacEnable, |
|
|
boolean |
xipEnable |
|
) |
| |
Switch Mode of the OSPI Driver Parameters (in) : boolean dacEnable - should DAC mode be enaled or disabled Parameters (in) : boolean xipEnable - should XIP mode be enaled or disabled Mode : Supervisor Mode (Privileged Mode)
◆ Fls_Init()
Initializes the Flash Driver.
* Service name : Fls_Init
* Syntax : void Fls_Init( const Fls_ConfigType* ConfigPtr )
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : 0x00
* Sync/Async : Synchronous
* Reentrancy : Non Reentrant
* Parameters (in) : ConfigPtr - Pointer to flash driver configuration set
* Parameters (inout) : None
* Parameters (out) : None
* Return value : None
* Description : Initializes the Flash Driver
*
◆ Fls_Erase()
Erases flash sector(s).
* Service name : Fls_Erase
* Syntax : Std_ReturnType Fls_Erase(Fls_AddressType TargetAddress
* ,Fls_LengthType Length)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : 0x01
* Sync/Async : Asynchronous
* Reentrancy : Non Reentrant
* Parameters (in) : TargetAddress - Target address in flash memory.
* This address offset will be added to the flash memory
* base address.
* Length - Number of bytes to erase
* Parameters (inout) : None
* Parameters (out) : None
* Return value : Std_ReturnType -
* E_OK: erase command has been accepted
* E_NOT_OK: erase command has not been accepted
* Description : Erases flash sector(s).
*
◆ Fls_Write()
Writes one or more complete flash pages.
* Service name : Fls_Write
* Syntax : Std_ReturnType Fls_Write(Fls_AddressType TargetAddress
* ,const uint8* SourceAddressPtr,
* Fls_LengthType Length)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : 0x02
* Sync/Async : Asynchronous
* Reentrancy : Non Reentrant
* Parameters (in) : TargetAddress - Target address in flash memory.
* This address offset will be added to the flash memory
* base address.
* SourceAddressPtr - Pointer to source data buffer
* Length - Number of bytes to erase
* Parameters (inout) : None
* Parameters (out) : None
* Return value : Std_ReturnType -
* E_OK: write command has been accepted
* E_NOT_OK: write command has not been accepted
* Description : Writes one or more complete flash pages.
*
◆ Fls_Read()
Reads from flash memory..
* Service name : Fls_Read
* Syntax : Std_ReturnType Fls_Read((Fls_AddressType SourceAddress
* ,const uint8* TargetAddressPtr,
* Fls_LengthType Length)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : 0x07
* Sync/Async : Asynchronous
* Reentrancy : Non Reentrant
* Parameters (in) : SourceAddress - source address in flash memory.
* This address offset will be added to the flash memory
* base address.
* TargetAddressPtr - Pointer to source data buffer
* Length - Number of bytes to erase
* Parameters (inout) : None
* Parameters (out) : None
* Return value : Std_ReturnType -
* E_OK: read command has been accepted
* E_NOT_OK: read command has not been accepted
* Description : Reads from flash memory.
*
◆ Fls_Compare()
Compares the contents of an area of flash memory with that of an application data buffer.
* Service name : Fls_Compare
* Syntax : Std_ReturnType Fls_Compare
* (Fls_AddressType SourceAddress,
* const uint8* TargetAddressPtr,
* Fls_LengthType Length)
* Mode : User Mode (Non-Privileged Mode)
* Service ID[hex] : 0x08
* Sync/Async : Asynchronous
* Reentrancy : Non Reentrant
* Parameters (in) : SourceAddress - Target address in flash memory.
* This address offset will be added to the flash memory
* base address.
* TargetAddressPtr - Pointer to source data buffer
* Length - Number of bytes to erase
* Parameters (inout) : None
* Parameters (out) : None
* Return value : Std_ReturnType -
* E_OK: compare command has been accepted
* E_NOT_OK: compare command has not been accepted
* Description : Compares the contents of an area of flash memory
* with that of an application data buffer.
*
◆ Fls_BlankCheck()
The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed.
* Service name : Fls_BlankCheck
* Syntax : Std_ReturnType Fls_Compare
* (Fls_AddressType TargetAddress,,
* Fls_LengthType Length)
* Mode : User Mode (Non-Privileged Mode)
* Service ID[hex] : 0x0a
* Sync/Async : Asynchronous
* Reentrancy : Non Reentrant
* Parameters (in) : TargetAddress - Target address in flash memory.
* This address offset will be added to the flash memory
* base address.
* SourceAddressPtr - Pointer to source data buffer
* Length - Number of bytes to erase
* Parameters (inout) : None
* Parameters (out) : None
* Return value : Std_ReturnType -
* E_OK: BlankCheck command has been accepted
* E_NOT_OK: BlankCheck command has not been accepted
* Description : The function Fls_BlankCheck shall verify,
* whether a given memory area has been
* erased but not (yet) programmed.
*
◆ Fls_GetStatus()
| MemIf_StatusType Fls_GetStatus |
( |
void |
| ) |
|
Returns the driver state.
* Service name : Fls_GetStatus
* Syntax : MemIf_StatusType Fls_GetStatus( void )
* Mode : User Mode (Non-Privileged Mode)
* Service ID[hex] : 0x04
* Sync/Async : Synchronous
* Reentrancy : Reentrant
* Parameters (in) : None
* Parameters (inout) : None
* Parameters (out) : None
* Return value : MemIf_StatusType
* Description : Returns the driver state.
*
◆ Fls_GetVersionInfo()
| Std_ReturnType Fls_GetVersionInfo |
( |
Std_VersionInfoType * |
versioninfo | ) |
|
This service returns the version information of this module.
* Service name : Fls_GetVersionInfo
* Syntax : void Fls_GetVersionInfo( Std_VersionInfoType*
* versioninfo )
* Mode : User Mode (Non-Privileged Mode)
* Service ID[hex] : 0x10
* Sync/Async : Synchronous
* Reentrancy : Reentrant
* Parameters (in) : None
* Parameters (inout) : versioninfo - Pointer to where to store the version
* information of this module
* Parameters (out) : None
* Return value : None
* Description : This service returns the version information of this
* module
*
◆ Fls_GetJobResult()
| MemIf_JobResultType Fls_GetJobResult |
( |
void |
| ) |
|
Returns the result of the last job.
* Service name : Fls_GetJobResult
* Syntax : MemIf_JobResultType Fls_GetJobResult(void)
* Mode : User Mode (Non-Privileged Mode)
* Service ID[hex] : 0x05
* Sync/Async : Synchronous
* Reentrancy : Reentrant
* Parameters (in) : None
* Parameters (inout) : None
* Parameters (out) : None
* Return value : MemIf_JobResultType
* Description : Returns the result of the last job.
*
◆ Fls_MainFunction()
| void Fls_MainFunction |
( |
void |
| ) |
|
Performs the processing of jobs.
* Service name : Fls_MainFunction
* Syntax : void Fls_MainFunction(void)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : 0x06
* Description : Performs the processing of jobs.
*
◆ Fls_Cancel()
Cancels an ongoing job.
* Service name : Fls_Cancel
* Syntax : void Fls_Cancel(void)
* Mode : User Mode (Non-Privileged Mode)
* Service ID[hex] : 0x03
* Sync/Async : Synchronous
* Reentrancy : Non Reentrant
* Parameters (in) : None
* Parameters (inout) : None
* Parameters (out) : None
* Return value : None
* Description : Cancels an ongoing job.
*