![]() |
MATHLIB User Guide
|
Go to the source code of this file.
Data Structures | |
| struct | MATHLIB_SESA1DSequential_t |
| Structure containing the initialization parameters for kernels involving 1D sequential access. More... | |
Macros | |
| #define | MATHLIB_TEST_OUTPUT_HEAP 0 |
| #define | MATHLIB_TEST_OUTPUT_MSMC 1 |
| #define | MATHLIB_DEBUGPRINT 0 |
| Enable debug printf statements. More... | |
| #define | MATHLIB_PRINTF(fmt, ...) |
| #define | MATHLIB_DEBUGPRINTFN(N, fmt, ...) |
Typedefs | |
| typedef MATHLIB_STATUS_NAME | MATHLIB_STATUS |
| Return value for MATHLIB functions. More... | |
Enumerations | |
| enum | MATHLIB_STATUS_NAME { MATHLIB_SUCCESS = 0 , MATHLIB_ERR_FAILURE = 1 , MATHLIB_ERR_INVALID_VALUE = 2 , MATHLIB_ERR_INVALID_TYPE = 3 , MATHLIB_ERR_INVALID_DIMENSION = 4 , MATHLIB_ERR_NULL_POINTER = 5 , MATHLIB_ERR_NOT_IMPLEMENTED = 6 , MATHLIB_ERR_NOT_EQUAL_WIDTH_STRIDE = 7 , MATHLIB_ERR_NOT_ALIGNED_PTRS_STRIDES = 8 , MATHLIB_ERR_NOT_ALIGNED_WIDTHS = 9 , MATHLIB_ERR_BUFFER_TOO_SMALL = 10 , MATHLIB_ERR_INVALID_ACTIVATION = 11 , MATHLIB_ERR_INVALID_SHIFT = 12 , MATHLIB_ERROR_MAX = 13 } |
| The enumeration of all status codes. More... | |
| enum | MATHLIB_data_type_e { MATHLIB_INT8 = 0 , MATHLIB_INT16 = 1 , MATHLIB_INT32 = 2 , MATHLIB_INT64 = 3 , MATHLIB_INT128 = 4 , MATHLIB_UINT8 = 5 , MATHLIB_UINT16 = 6 , MATHLIB_UINT24 = 7 , MATHLIB_UINT32 = 8 , MATHLIB_UINT64 = 9 , MATHLIB_UINT128 = 10 , MATHLIB_FLOAT16 = 11 , MATHLIB_FLOAT32 = 12 , MATHLIB_FLOAT64 = 13 } |
| Enum of all datatypes. More... | |
| #define MATHLIB_TEST_OUTPUT_HEAP 0 |
Definition at line 63 of file MATHLIB_types.h.
| #define MATHLIB_TEST_OUTPUT_MSMC 1 |
Definition at line 71 of file MATHLIB_types.h.
| #define MATHLIB_DEBUGPRINT 0 |
Enable debug printf statements.
Definition at line 80 of file MATHLIB_types.h.
| #define MATHLIB_PRINTF | ( | fmt, | |
| ... | |||
| ) |
Definition at line 83 of file MATHLIB_types.h.
| #define MATHLIB_DEBUGPRINTFN | ( | N, | |
| fmt, | |||
| ... | |||
| ) |
Definition at line 98 of file MATHLIB_types.h.