MATHLIB User Guide
MATHLIB_sqrt.h File Reference

Go to the source code of this file.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_sqrt (size_t length, T *pSrc, T *pDst)
 Performs the elementwise square root of an input vectors. Function can be overloaded with float and double pointers, and the appropriate precision is employed to compute elementwise square root of an input vector. More...
 
MATHLIB_STATUS MATHLIB_sqrt_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_sqrt. Function accepts float pointers. More...
 
MATHLIB_STATUS MATHLIB_sqrt_dp (size_t length, double *pSrc, double *pDst)
 This function is the C interface for MATHLIB_sqrt. Function accepts double pointers. More...