MATHLIB User Guide
MATHLIB_lut.h File Reference

Go to the source code of this file.

Macros

#define MATHLIB_KTABLE_OFFSET   0
 
#define MATHLIB_JTABLE_OFFSET   4
 
#define MATHLIB_LOGTABLE_OFFSET   8
 
#define MATHLIB_VTABLE_OFFSET   16
 

Functions

template<typename vecType >
static c7x::uint_vec MATHLIB_LUTReadUpperBits (vecType vecOffset)
 This method reads bits 63-32 of LUT value at vecOffset. More...
 
template<typename vecType >
static c7x::uint_vec MATHLIB_LUTReadLowerBits (vecType vecOffset)
 This method reads bits 31-0 of LUT value at vecOffset. More...
 
static void MATHLIB_LUTInit ()
 This method intializes the upper and lower bit lookup tables. More...