MATHLIB User Guide
MATHLIB_exp.h File Reference

Go to the source code of this file.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_exp (size_t length, T *pSrc, T *pDst)
 Performs the elementwise exponentialization of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise exponentialization of the input vector. More...
 
MATHLIB_STATUS MATHLIB_exp_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_exp. Function accepts float pointers. More...