MATHLIB User Guide
MATHLIB_exp10.h File Reference

Go to the source code of this file.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_exp10 (size_t length, T *pSrc, T *pDst)
 Performs the elementwise 10^x for all x in the input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise exponentialization of the input vector. More...
 
MATHLIB_STATUS MATHLIB_exp10_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_exp10. Function accepts float pointers. More...