MATHLIB User Guide
MATHLIB_cos.cpp File Reference

Go to the source code of this file.

Macros

#define ELEMENT_COUNT(x)   c7x::element_count_of<x>::value
 

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_cos (size_t length, T *pSrc, T *pDst)
 
template<>
MATHLIB_STATUS MATHLIB_cos< float > (size_t length, float *pSrc, float *pDst)
 
template<>
MATHLIB_STATUS MATHLIB_cos< double > (size_t length, double *pSrc, double *pDst)
 
MATHLIB_STATUS MATHLIB_cos_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_cos. Function accepts float pointers. More...
 
MATHLIB_STATUS MATHLIB_cos_dp (size_t length, double *pSrc, double *pDst)
 This function is the C interface for MATHLIB_cos. Function accepts double pointers. More...
 

Macro Definition Documentation

◆ ELEMENT_COUNT

#define ELEMENT_COUNT (   x)    c7x::element_count_of<x>::value

Definition at line 34 of file MATHLIB_cos.cpp.

Function Documentation

◆ MATHLIB_cos()

template<typename T >
MATHLIB_STATUS MATHLIB_cos ( size_t  length,
T *  pSrc,
T *  pDst 
)

◆ MATHLIB_cos< float >()

template<>
MATHLIB_STATUS MATHLIB_cos< float > ( size_t  length,
float *  pSrc,
float *  pDst 
)

Definition at line 54 of file MATHLIB_cos.cpp.

◆ MATHLIB_cos< double >()

template<>
MATHLIB_STATUS MATHLIB_cos< double > ( size_t  length,
double *  pSrc,
double *  pDst 
)

Definition at line 184 of file MATHLIB_cos.cpp.