TI J721E Imaging User Guide
IssSensor_CreateParams Struct Reference

Detailed Description

Create Time parameters, ISS sensor layer uses these parameters and configures board module and sensor.

Data Fields

char name [ISS_SENSORS_MAX_NAME]
 
uint16_t i2cInstId
 
uint8_t i2cAddrSensor [ISS_SENSORS_MAX_CHANNEL]
 
uint8_t i2cAddrSer [ISS_SENSORS_MAX_CHANNEL]
 
IssSensor_Info sensorInfo
 
uint32_t num_channels
 
uint32_t dccId
 

Field Documentation

◆ name

char IssSensor_CreateParams::name[ISS_SENSORS_MAX_NAME]

Name of the sensor

◆ i2cInstId

uint16_t IssSensor_CreateParams::i2cInstId

I2C Instance id for the sensor

◆ i2cAddrSensor

uint8_t IssSensor_CreateParams::i2cAddrSensor[ISS_SENSORS_MAX_CHANNEL]

I2C alias addresses for the sensor

◆ i2cAddrSer

uint8_t IssSensor_CreateParams::i2cAddrSer[ISS_SENSORS_MAX_CHANNEL]

I2C alias addresses for the serializer

◆ sensorInfo

IssSensor_Info IssSensor_CreateParams::sensorInfo

< I2C Address of misc part on the camera board Sensor Information e.g. width, height, format etc.

◆ num_channels

uint32_t IssSensor_CreateParams::num_channels

Number of channels supported

◆ dccId

uint32_t IssSensor_CreateParams::dccId

camera identifier