FFTLIB User Guide
FFTLIB_FFT_dftSmall_ixX_cxX_oxX_priv.h
Go to the documentation of this file.
1 /******************************************************************************
2 * *
3 * module name :FFTLIB *
4 * *
5 * module descripton :Matrix Multiply Accelerator Library module for C7x+MMA *
6 * *
7 * Copyright (C) 2017-2018 Texas Instruments Incorporated - https://www.ti.com/ *
8 * ALL RIGHTS RESERVED *
9 * *
10 ******************************************************************************/
11 
12 /********************************************************************************
13  * @file FFTLIB_FFTLIB__dftSmall_ixX_cxX_oxX_priv.h
14  *
15  * @brief File to hold private parameter of function FFTLIB_FFT_dftSmall
16  *
17  * @version 0.1 - Jan 2018 : Initial Version
18  *
19  ********************************************************************************/
20 
21 #ifndef FFTLIB_FFT_DFTSMALL_IXX_CXX_OXX_PRIV_H_
22 #define FFTLIB_FFT_DFTSMALL_IXX_CXX_OXX_PRIV_H_
23 
25 #include "../../common/FFTLIB_utility.h"
26 
38 #define FFTLIB_FFT_DFTSMALL_IXX_CXX_OXX_PBLOCK_SIZE (3*SE_PARAM_SIZE + 1*FFTLIB_PARAM_SIZE + sizeof(int32_t))
39 
47  FFTLIB_kernelHandle handle,
48  const void *restrict pX,
49  const void *restrict pW,
50  void *restrict pY);
51 
81 template <uint32_t dataType>
83  FFTLIB_kernelHandle handle,
84  const FFTLIB_bufParams1D_t *bufParamsX,
85  const FFTLIB_bufParams1D_t *bufParamsW,
86  const FFTLIB_bufParams1D_t *bufParamsY,
87  const FFTLIB_FFT_dftSmall_ixX_cxX_oxX_InitArgs *pKerInitArgs);
88 
123 template <typename dataType, uint32_t MMA_SIZE>
125  FFTLIB_kernelHandle handle,
126  const void *restrict pX,
127  const void *restrict pW,
128  void *restrict pY);
129 
147 template <typename dataType, typename accumulateType, uint32_t MMA_SIZE>
149  FFTLIB_kernelHandle handle,
150  const void *restrict pX,
151  const void *restrict pW,
152  void *restrict pY);
153 
169 template <typename dataType>
171  const FFTLIB_FFT_dftSmall_ixX_cxX_oxX_InitArgs * pKerInitArgs,
172  void *restrict pW,
173  const FFTLIB_bufParams1D_t * bufParamsW);
174 
193 template <uint32_t dataType>
195  const FFTLIB_FFT_dftSmall_ixX_cxX_oxX_InitArgs * pKerInitArgs,
196  FFTLIB_bufParams1D_t * bufParamsX,
197  FFTLIB_bufParams1D_t * bufParamsW,
198  FFTLIB_bufParams1D_t * bufParamsY);
199 
203 typedef struct
204 {
217 
238  FFTLIB_kernelHandle handle,
239  FFTLIB_bufParams1D_t *bufParamsX,
240  FFTLIB_bufParams1D_t *bufParamsW,
241  FFTLIB_bufParams1D_t *bufParamsY,
243 
244 #endif /* FFTLIB_FFT_DFTSMALL_IXX_CXX_OXX_PRIV_H_ */
245 
246 /* ======================================================================== */
247 /* End of file: FFTLIB_FFT_dftSmall_ixX_cxX_oxX.h */
248 /* ======================================================================== */
249 
FFTLIB_STATUS FFTLIB_FFT_dftSmall_ixX_cxX_oxX_init_cn(FFTLIB_kernelHandle handle, FFTLIB_bufParams1D_t *bufParamsX, FFTLIB_bufParams1D_t *bufParamsW, FFTLIB_bufParams1D_t *bufParamsY, FFTLIB_FFT_dftSmall_ixX_cxX_oxX_InitArgs *pKerInitArgs)
This function is the initialization function for the natural C implementation of the kernel....
FFTLIB_STATUS FFTLIB_FFT_dftSmall_ixX_cxX_oxX_exec_ci(FFTLIB_kernelHandle handle, const void *restrict pX, const void *restrict pW, void *restrict pY)
This function is the main execution function for the C7x implementation of the kernel....
FFTLIB_STATUS(* pFxnFFTLIB_FFT_dftSmall_ixX_cxX_oxX_exec)(FFTLIB_kernelHandle handle, const void *restrict pX, const void *restrict pW, void *restrict pY)
This is a function pointer type that conforms to the declaration of FFTLIB_FFT_dftSmall_ixX_cxX_oxX_e...
FFTLIB_STATUS FFTLIB_FFT_dftSmall_ixX_cxX_oxX_init_ci(FFTLIB_kernelHandle handle, const FFTLIB_bufParams1D_t *bufParamsX, const FFTLIB_bufParams1D_t *bufParamsW, const FFTLIB_bufParams1D_t *bufParamsY, const FFTLIB_FFT_dftSmall_ixX_cxX_oxX_InitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
#define FFTLIB_FFT_DFTSMALL_IXX_CXX_OXX_PBLOCK_SIZE
Macro to define the size of bufPblock array of FFTLIB_FFT_dftSmall_ixX_cxX_oxX_PrivArgs structure.
FFTLIB_STATUS FFTLIB_FFT_dftSmall_ixX_cxX_oxX_exec_cn(FFTLIB_kernelHandle handle, const void *restrict pX, const void *restrict pW, void *restrict pY)
This function is the main execution function for the natural C implementation of the kernel....
FFTLIB_STATUS FFTLIB_FFT_dftSmall_ixX_cxX_oxX_twGen(const FFTLIB_FFT_dftSmall_ixX_cxX_oxX_InitArgs *pKerInitArgs, void *restrict pW, const FFTLIB_bufParams1D_t *bufParamsW)
This is a utility function that generates the DFT computational matrix into the provided buffer.
void * FFTLIB_kernelHandle
Handle type for FFTLIB operations.
Definition: FFTLIB_types.h:217
FFTLIB_STATUS_NAME
The enumeration of all status codes.
Definition: FFTLIB_types.h:172
FFTLIB_STATUS_NAME FFTLIB_STATUS
Return value for FFTLIB functions.
Definition: FFTLIB_types.h:215
FFTLIB_STATUS FFTLIB_FFT_dftSmall_ixX_cxX_oxX_getSizes(const FFTLIB_FFT_dftSmall_ixX_cxX_oxX_InitArgs *pKerInitArgs, FFTLIB_bufParams1D_t *bufParamsX, FFTLIB_bufParams1D_t *bufParamsW, FFTLIB_bufParams1D_t *bufParamsY)
This function is a utility function that the application calls to obtain the sizes of data buffers.
Structure containing the parameters for DFT computation.
Structure that is reserved for internal use by the kernel.
pFxnFFTLIB_FFT_dftSmall_ixX_cxX_oxX_exec execute
Function pointer to point to the right execution variant between FFTLIB_FFT_dftSmall_ixX_cxX_oxX_exec...
FFTLIB_FFT_dftSmall_ixX_cxX_oxX_InitArgs initArgs
Structure holding initialization parameters
A structure for a 1 dimensional buffer descriptor.