![]() |
ETHFW API Guide
|
Request params for ETHREMOTECFG_CMD_REGISTER_MAC or ETHREMOTECFG_CMD_DEREGISTER_MAC commands.
This structure holds the MAC address and the RxflowId which needs to be registered for a given virtual port.
Data Fields | |
| EthRemoteCfg_ReqHdr | hdr |
| uint8_t | macAddr [ETHREMOTECFG_MACADDRLEN] |
| uint32_t | flowIdxBase |
| uint32_t | flowIdxOffset |
| EthRemoteCfg_ReqHdr EthRemoteCfg_MacAddrRxFlowReq::hdr |
Request message common header.
| uint8_t EthRemoteCfg_MacAddrRxFlowReq::macAddr[ETHREMOTECFG_MACADDRLEN] |
MAC address which needs to be registered.
| uint32_t EthRemoteCfg_MacAddrRxFlowReq::flowIdxBase |
Rx flow index base.
| uint32_t EthRemoteCfg_MacAddrRxFlowReq::flowIdxOffset |
Rx flow index offset to which the MAC address needs to be registered.