DSPLIB User Guide
DSPLIB_mulConstant_PrivArgs Struct Reference

Detailed Description

Structure that is reserved for internal use by the kernel.

Definition at line 137 of file DSPLIB_mulConstant_priv.h.

Data Fields

pFxnDSPLIB_mulConstant_exec execute
 Function pointer to point to the right execution variant between DSPLIB_mulConstant_exec_cn and DSPLIB_mulConstant_exec_ci.
More...
 
int32_t blockSize
 Size of input buffer for different batches DSPLIB_mulConstant_init that will be retrieved and used by DSPLIB_mulConstant_exec
More...
 
uint8_t bufPblock [DSPLIB_MULCONSTANT_IXX_IXX_OXX_PBLOCK_SIZE]
 

Field Documentation

◆ execute

pFxnDSPLIB_mulConstant_exec DSPLIB_mulConstant_PrivArgs::execute

Function pointer to point to the right execution variant between DSPLIB_mulConstant_exec_cn and DSPLIB_mulConstant_exec_ci.

Definition at line 141 of file DSPLIB_mulConstant_priv.h.

◆ blockSize

int32_t DSPLIB_mulConstant_PrivArgs::blockSize

Size of input buffer for different batches DSPLIB_mulConstant_init that will be retrieved and used by DSPLIB_mulConstant_exec

Definition at line 145 of file DSPLIB_mulConstant_priv.h.

◆ bufPblock

uint8_t DSPLIB_mulConstant_PrivArgs::bufPblock[DSPLIB_MULCONSTANT_IXX_IXX_OXX_PBLOCK_SIZE]

Definition at line 146 of file DSPLIB_mulConstant_priv.h.