![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 164 of file DSPLIB_cholesky_solver_priv.h.
Data Fields | |
| pFxnDSPLIB_cholesky_solver_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_cholesky_solver_exec_cn and DSPLIB_cholesky_solver_exec_ci. More... | |
| int32_t | order |
| Order of input buffer for different batches DSPLIB_cholesky_solver_init that will be retrieved and used by DSPLIB_cholesky_solver_exec More... | |
| int32_t | stride |
| int32_t | strideCn |
| uint8_t | bufPblock [DSPLIB_CHOLESKY_SOLVER_IXX_IXX_OXX_PBLOCK_SIZE] |
| DSPLIB_matTrans_PrivArgs | matTransPrivArgs |
| Struture to store privArgs for matTrans kernel. More... | |
| pFxnDSPLIB_cholesky_solver_exec DSPLIB_cholesky_solver_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_cholesky_solver_exec_cn and DSPLIB_cholesky_solver_exec_ci.
Definition at line 168 of file DSPLIB_cholesky_solver_priv.h.
| int32_t DSPLIB_cholesky_solver_PrivArgs::order |
Order of input buffer for different batches DSPLIB_cholesky_solver_init that will be retrieved and used by DSPLIB_cholesky_solver_exec
Definition at line 172 of file DSPLIB_cholesky_solver_priv.h.
| int32_t DSPLIB_cholesky_solver_PrivArgs::stride |
Definition at line 173 of file DSPLIB_cholesky_solver_priv.h.
| int32_t DSPLIB_cholesky_solver_PrivArgs::strideCn |
Definition at line 174 of file DSPLIB_cholesky_solver_priv.h.
| uint8_t DSPLIB_cholesky_solver_PrivArgs::bufPblock[DSPLIB_CHOLESKY_SOLVER_IXX_IXX_OXX_PBLOCK_SIZE] |
Definition at line 175 of file DSPLIB_cholesky_solver_priv.h.
| DSPLIB_matTrans_PrivArgs DSPLIB_cholesky_solver_PrivArgs::matTransPrivArgs |
Struture to store privArgs for matTrans kernel.
Definition at line 177 of file DSPLIB_cholesky_solver_priv.h.