|
| int32_t | DSPLIB_svd_small_getHandleSize (DSPLIB_svd_small_InitArgs *pKerInitArgs) |
| | This is a query function to calculate the size of internal handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_svd_small_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsA, const DSPLIB_bufParams2D_t *bufParamsU, const DSPLIB_bufParams2D_t *bufParamsV, const DSPLIB_bufParams1D_t *bufParamsDiag, const DSPLIB_bufParams1D_t *bufParamsSuperDiag, const DSPLIB_svd_small_InitArgs *pKerInitArgs) |
| | This function checks the validity of the parameters passed to DSPLIB_svd_small_init function. This function is called with the same parameters as the DSPLIB_svd_small_init, and this function must be called before the DSPLIB_svd_small_init is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_svd_small_init (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsA, const DSPLIB_bufParams2D_t *bufParamsU, const DSPLIB_bufParams2D_t *bufParamsV, const DSPLIB_bufParams1D_t *bufParamsDiag, const DSPLIB_bufParams1D_t *bufParamsSuperDiag, const DSPLIB_svd_small_InitArgs *pKerInitArgs) |
| | This function should be called before the DSPLIB_svd_small_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine and streaming address generator. The results of these operations are stored in the handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_svd_small_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pU, const void *restrict pV, const void *restrict pDiag, const void *restrict pSuperDiag, const void *restrict pU1) |
| | This function checks the validity of the parameters passed to DSPLIB_svd_small_exec function. This function is called with the same parameters as the DSPLIB_svd_small_exec, and this function must be called before the DSPLIB_svd_small_exec is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_svd_small_exec (DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pU, void *restrict pV, void *restrict pDiag, void *restrict pSuperDiag, void *restrict pU1) |
| | This function is the main kernel compute function. More...
|
| |