![]() |
DSPLIB User Guide
|
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_svd.
Definition in file DSPLIB_svd_priv.h.
Go to the source code of this file.
Data Structures | |
| struct | DSPLIB_svd_PrivArgs |
| Structure that is reserved for internal use by the kernel. More... | |
Macros | |
| #define | DSPLIB_SVD_IXX_IXX_OXX_PBLOCK_SIZE (26 * SE_PARAM_SIZE) |
| Macro to define the size of bufPblock array of DSPLIB_svd_PrivArgs structure. More... | |
Typedefs | |
| typedef DSPLIB_STATUS(* | pFxnDSPLIB_svd_exec) (DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pU, void *restrict pV, void *restrict pDiag, void *restrict pSuperDiag, void *restrict pU1, void *restrict pV1, void *restrict pScratch) |
| This is a function pointer type that conforms to the declaration of DSPLIB_svd_exec_ci and DSPLIB_svd_exec_cn. More... | |
Functions | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_svd_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsU, const DSPLIB_bufParams2D_t *bufParamsV, const DSPLIB_bufParams1D_t *bufParamsDiag, const DSPLIB_bufParams1D_t *bufParamsSuperDiag, const DSPLIB_svdInitArgs *pKerInitArgs) |
| This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_svd_init. More... | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_svd_exec_ci (DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pU, void *restrict pV, void *restrict pDiag, void *restrict pSuperDiag, void *restrict pU1, void *restrict pV1, void *restrict pScratch) |
| This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_svd_exec. More... | |
| DSPLIB_STATUS | DSPLIB_svd_init_cn (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsU, const DSPLIB_bufParams2D_t *bufParamsV, const DSPLIB_bufParams1D_t *bufParamsDiag, const DSPLIB_bufParams1D_t *bufParamsSuperDiag, const DSPLIB_svdInitArgs *pKerInitArgs) |
| This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_svd_init. More... | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_svd_exec_cn (DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pU, void *restrict pV, void *restrict pDiag, void *restrict pSuperDiag, void *restrict pU1, void *restrict pV1, void *restrict pScratch) |
| This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_svd_exec. More... | |
| template<typename dataType > | |
| void | uColProcess (dataType *U, int32_t Nrows, int32_t Ncols, int32_t colUStride, dataType half_norm_squared, dataType *U1, dataType scale, uint8_t *pBlock) |
| template<typename dataType > | |
| dataType | DSPLIB_bidiag_uCol_halfnorm_ci (dataType *U, int32_t Nrows, int32_t Ncols, int32_t colUStride, dataType *half_norm_squared, dataType *U1, dataType *s, uint8_t *pBlock) |
| This function calculates the half-norms corresponding to the column of input matrix U and returns scale. More... | |
| template<typename dataType > | |
| dataType | DSPLIB_bidiag_uRow_halfnorm_ci (dataType *U, int32_t Nrows, int32_t Ncols, int32_t colUStride, dataType *half_norm_squared, dataType *U1, dataType *s, dataType *superdiag, uint8_t *pBlock) |
| This function calculates the half-norm corresponding to the row of input matrix U and returns scale. More... | |
| template<typename dataType > | |
| void | uRowProcess (dataType *U, int32_t Nrows, int32_t Ncols, int32_t colUStride, dataType *superdiag, dataType *U1, dataType scale, uint8_t *pBlock) |
| template<typename dataType > | |
| void | vColProcess (dataType *V, int32_t Nrows, int32_t Ncols, int32_t colVStride, dataType s, dataType *U1, dataType *U, int32_t colUStride, uint8_t *PBlock) |
| template<typename dataType > | |
| void | DSPLIB_bidiag_uFinal_expand_ci (dataType *U, int32_t Nrows, int32_t Ncols, int32_t colUStride, uint8_t *pBlock) |
| This function expands columns of U matrix to get a square matrix and fill the columns with '0' values. More... | |
| template<typename dataType > | |
| void | uSiUpdate (dataType *U, int32_t Nrows, int32_t Ncols, int32_t colUStride, dataType s, dataType *U1, uint8_t *pBlock) |
| template<typename dataType > | |
| void | DSPLIB_bidiag_uFinal_normalize_ci (dataType *U, int32_t Nrows, dataType s, int32_t colUStride, uint8_t *pBlock) |
| This function normalizes the column of input matrix U. More... | |
| template<typename dataType > | |
| void | DSPLIB_bidiag_uFinal_initalize_ci (dataType *U, int32_t Nrows, int32_t Ncols, int32_t colUStride, dataType s, dataType *U1, uint8_t *pBlock) |
| This function implements the process corresponding to the "initial U" loop in natural implementation. More... | |
| template<typename dataType > | |
| void | DSPLIB_diag_proc_ci (dataType *V, int32_t startRow, int32_t Nrows, int32_t Ncols, int32_t rowVStride, dataType *cV, dataType *sV, uint8_t *pBlock) |
| Updates rows of V' and U' based on the precalculated cV/cU and sV/sU vectors. More... | |
| template<typename dataType > | |
| void | DSPLIB_singularSort_swap_ci (dataType *V, int32_t Nrows, int32_t Ncols, int32_t rowVStride, int32_t *sortIndex, dataType *vBuff, uint8_t *pBlock) |
| This function uses the max index values calculated from DSPLIB_singularSort_index_ci to shuffle the rows of U' and V' matrix (i.e. colums of U and V matrix). More... | |
| template<typename dataType > | |
| void | DSPLIB_bidiag_uCol_ci (dataType *U, int32_t Nrows, int32_t Ncols, int32_t colUStride, dataType half_norm_squared, dataType *U1, dataType scale, uint8_t *pBlock) |
| This function implements the Household processing on columns of input U matrix corresponding to the natural implementation. More... | |
| template<typename dataType > | |
| void | DSPLIB_bidiag_uRow_ci (dataType *U, int32_t Nrows, int32_t Ncols, int32_t colUStride, dataType *superdiag, dataType *U1, dataType scale, uint8_t *pBlock) |
| This function implements the Household processing on rows of input U matrix corresponding to the natural implementation. More... | |
| template<typename dataType > | |
| void | DSPLIB_bidiag_uFinal_ci (dataType *U, int32_t Nrows, int32_t Ncols, int32_t colUStride, dataType s, dataType *U1, uint8_t *pBlock) |
| This function implements the process corresponding to the "update U" loop in natural implementation. More... | |
| template<typename dataType > | |
| void | DSPLIB_bidiag_v_ci (dataType *V, int32_t Nrows, int32_t Ncols, int32_t colVStride, dataType s, dataType *U1, dataType *U, int32_t colUStride, uint8_t *pBlock) |
| This function implements the process corresponding to the "update V" loop in natural implementation. More... | |
| template<typename dataType > | |
| void | DSPLIB_diag_negate_v_ci (dataType *V, int32_t Ncols, int32_t colVStride, uint8_t *pBlock) |
| Negates the values of a row in V. More... | |
| template<typename dataType > | |
| void | DSPLIB_diag_epsilon_ci (dataType *diag, dataType *superdiag, dataType *epsilon, int32_t Ncols, uint8_t *pBlock) |
| Updates "epsilon" value based on absolute max values from "diag" and "superdiag" vectors. More... | |
| template<typename dataType > | |
| void | DSPLIB_diag_rotation_check_ci (dataType *diag, dataType *superdiag, dataType epsilon, int32_t *m, int32_t *rotation_test, int32_t Ncols, uint8_t *pBlock) |
| Updates values of "m" and "rotation_test" flag vased on the values present in "diag", "superdiag" and "epsilon". More... | |
| template<typename dataType > | |
| void | DSPLIB_diag_rotation_proc_ci (dataType *U, int32_t startRow, int32_t Nrows, int32_t Ncols, int32_t rowUStride, dataType *cU, dataType *sU, uint8_t *pBlock) |
| Updates rows of U' based on the precalculated cU and sU vectors. More... | |
| template<typename dataType > | |
| void | DSPLIB_singularSort_index_ci (dataType *singular_values, dataType *singularBuffer, int32_t *maxIndArr, int32_t Ncols, uint8_t *pBlock) |
| This function sorts the singular values in descending order and also records the max index values for shuffling of U and V matrix columns. More... | |
| template<typename dataType > | |
| void | DSPLIB_diag_sqrt_ci (dataType *superdiag, dataType *diag, int32_t length, uint8_t *pBlock) |
| Calculates the reciprocal of square-roots of "diag" and "superdiag" vectors. More... | |
| template<typename dataType > | |
| void | DSPLIB_svd_blk_move_ci (dataType *pOut, dataType *pIn, int32_t Nrows, int32_t Ncols, int32_t colOutStride, int32_t colInStride, uint8_t *pBlock) |
| Copy input matrix pIn to pOut. More... | |
| template<typename dataType > | |
| void | DSPLIB_bidiag_uFinal_init_ci (DSPLIB_kernelHandle handle) |
| template<typename dataType > | |
| void | DSPLIB_diag_proc_init_ci (DSPLIB_kernelHandle handle) |
| template<typename dataType > | |
| void | DSPLIB_singularSort_swap_init_ci (DSPLIB_kernelHandle handle) |
| template<typename dataType > | |
| void | DSPLIB_bidiag_u_init_ci (DSPLIB_kernelHandle handle) |
| template<typename dataType > | |
| void | DSPLIB_bidiag_v_init_ci (DSPLIB_kernelHandle handle) |
| template<typename dataType > | |
| void | DSPLIB_svd_matTrans_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_svdInitArgs *kerInitArgs) |
| template<typename dataType > | |
| dataType | getRecip (dataType value) |
| template float | getRecip (float value) |
| template double | getRecip (double value) |
| #define DSPLIB_SVD_IXX_IXX_OXX_PBLOCK_SIZE (26 * SE_PARAM_SIZE) |
Macro to define the size of bufPblock array of DSPLIB_svd_PrivArgs structure.
Definition at line 40 of file DSPLIB_svd_priv.h.
| typedef DSPLIB_STATUS(* pFxnDSPLIB_svd_exec) (DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pU, void *restrict pV, void *restrict pDiag, void *restrict pSuperDiag, void *restrict pU1, void *restrict pV1, void *restrict pScratch) |
This is a function pointer type that conforms to the declaration of DSPLIB_svd_exec_ci and DSPLIB_svd_exec_cn.
Definition at line 47 of file DSPLIB_svd_priv.h.
| DSPLIB_STATUS DSPLIB_svd_init_ci | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams2D_t * | bufParamsU, | ||
| const DSPLIB_bufParams2D_t * | bufParamsV, | ||
| const DSPLIB_bufParams1D_t * | bufParamsDiag, | ||
| const DSPLIB_bufParams1D_t * | bufParamsSuperDiag, | ||
| const DSPLIB_svdInitArgs * | pKerInitArgs | ||
| ) |
This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_svd_init.
This function determines the configuration for the streaming engine resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_svd_exec_ci would be called later independently by the application. When DSPLIB_svd_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_svd_exec_ci does not lose cycles to determine the hardware configuration.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsU | : Pointer to the structure containing dimensional information of output buffer U |
| [out] | bufParamsV | : Pointer to the structure containing dimensional information of output buffer V |
| [out] | bufParamsDiag | : Pointer to the structure containing dimensional information of output buffer Diag |
| [out] | bufParamsSuperDiag | : Pointer to the structure containing dimensional information of output buffer SuperDiag |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 64 of file DSPLIB_svd_ci.cpp.
| DSPLIB_STATUS DSPLIB_svd_exec_ci | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pA, | ||
| void *restrict | pU, | ||
| void *restrict | pV, | ||
| void *restrict | pDiag, | ||
| void *restrict | pSuperDiag, | ||
| void *restrict | pU1, | ||
| void *restrict | pV1, | ||
| void *restrict | pScratch | ||
| ) |
This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_svd_exec.
| [in] | handle | : Active handle to the kernel |
| [in] | pA | : Pointer to the input buffer pA |
| [out] | pU | : Pointer to the output buffer pU |
| [out] | pV | : Pointer to the output buffer pV |
| [out] | pDiag | : Pointer to the output buffer pDiag |
| [out] | pSuperDiag | : Pointer to the output buffer pSuperDiag |
| [in] | pU1 | : Pointer to the buffer pU1 |
| [in] | pV1 | : Pointer to the buffer pV1 |
| [out] | pScratch | : Pointer to the buffer pScratch |
Definition at line 612 of file DSPLIB_svd_ci.cpp.
| DSPLIB_STATUS DSPLIB_svd_init_cn | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams2D_t * | bufParamsU, | ||
| const DSPLIB_bufParams2D_t * | bufParamsV, | ||
| const DSPLIB_bufParams1D_t * | bufParamsDiag, | ||
| const DSPLIB_bufParams1D_t * | bufParamsSuperDiag, | ||
| const DSPLIB_svdInitArgs * | pKerInitArgs | ||
| ) |
This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_svd_init.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsU | : Pointer to the structure containing dimensional information of output buffer U |
| [out] | bufParamsV | : Pointer to the structure containing dimensional information of output buffer V |
| [out] | bufParamsDiag | : Pointer to the structure containing dimensional information of output buffer Diag |
| [out] | bufParamsSuperDiag | : Pointer to the structure containing dimensional information of output buffer SuperDiag |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 62 of file DSPLIB_svd_cn.cpp.
| DSPLIB_STATUS DSPLIB_svd_exec_cn | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pA, | ||
| void *restrict | pU, | ||
| void *restrict | pV, | ||
| void *restrict | pDiag, | ||
| void *restrict | pSuperDiag, | ||
| void *restrict | pU1, | ||
| void *restrict | pV1, | ||
| void *restrict | pScratch | ||
| ) |
This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_svd_exec.
| [in] | handle | : Active handle to the kernel |
| [in] | pA | : Pointer to the input buffer pA |
| [out] | pU | : Pointer to the output buffer pU |
| [out] | pV | : Pointer to the output buffer pV |
| [out] | pDiag | : Pointer to the output buffer pDiag |
| [out] | pSuperDiag | : Pointer to the output buffer pSuperDiag |
| [in] | pU1 | : Pointer to the buffer pU1 |
| [in] | pV1 | : Pointer to the buffer pV1 |
| [out] | pScratch | : Pointer to the buffer pScratch |
Definition at line 746 of file DSPLIB_svd_cn.cpp.
| void uColProcess | ( | dataType * | U, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colUStride, | ||
| dataType | half_norm_squared, | ||
| dataType * | U1, | ||
| dataType | scale, | ||
| uint8_t * | pBlock | ||
| ) |
| dataType DSPLIB_bidiag_uCol_halfnorm_ci | ( | dataType * | U, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colUStride, | ||
| dataType * | half_norm_squared, | ||
| dataType * | U1, | ||
| dataType * | s, | ||
| uint8_t * | pBlock | ||
| ) |
This function calculates the half-norms corresponding to the column of input matrix U and returns scale.
Definition at line 172 of file DSPLIB_svd_bidiag_uMat_ci.cpp.
| dataType DSPLIB_bidiag_uRow_halfnorm_ci | ( | dataType * | U, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colUStride, | ||
| dataType * | half_norm_squared, | ||
| dataType * | U1, | ||
| dataType * | s, | ||
| dataType * | superdiag, | ||
| uint8_t * | pBlock | ||
| ) |
This function calculates the half-norm corresponding to the row of input matrix U and returns scale.
Definition at line 959 of file DSPLIB_svd_bidiag_uMat_ci.cpp.
| void uRowProcess | ( | dataType * | U, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colUStride, | ||
| dataType * | superdiag, | ||
| dataType * | U1, | ||
| dataType | scale, | ||
| uint8_t * | pBlock | ||
| ) |
| void vColProcess | ( | dataType * | V, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colVStride, | ||
| dataType | s, | ||
| dataType * | U1, | ||
| dataType * | U, | ||
| int32_t | colUStride, | ||
| uint8_t * | PBlock | ||
| ) |
| void DSPLIB_bidiag_uFinal_expand_ci | ( | dataType * | U, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colUStride, | ||
| uint8_t * | pBlock | ||
| ) |
This function expands columns of U matrix to get a square matrix and fill the columns with '0' values.
Definition at line 127 of file DSPLIB_svd_bidiag_uFinal_ci.cpp.
| void uSiUpdate | ( | dataType * | U, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colUStride, | ||
| dataType | s, | ||
| dataType * | U1, | ||
| uint8_t * | pBlock | ||
| ) |
| void DSPLIB_bidiag_uFinal_normalize_ci | ( | dataType * | U, |
| int32_t | Nrows, | ||
| dataType | s, | ||
| int32_t | colUStride, | ||
| uint8_t * | pBlock | ||
| ) |
This function normalizes the column of input matrix U.
Definition at line 328 of file DSPLIB_svd_bidiag_uFinal_ci.cpp.
| void DSPLIB_bidiag_uFinal_initalize_ci | ( | dataType * | U, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colUStride, | ||
| dataType | s, | ||
| dataType * | U1, | ||
| uint8_t * | pBlock | ||
| ) |
This function implements the process corresponding to the "initial U" loop in natural implementation.
Definition at line 187 of file DSPLIB_svd_bidiag_uFinal_ci.cpp.
| void DSPLIB_diag_proc_ci | ( | dataType * | V, |
| int32_t | startRow, | ||
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | rowVStride, | ||
| dataType * | cV, | ||
| dataType * | sV, | ||
| uint8_t * | pBlock | ||
| ) |
Updates rows of V' and U' based on the precalculated cV/cU and sV/sU vectors.
Definition at line 413 of file DSPLIB_svd_diag_ci.cpp.
| void DSPLIB_singularSort_swap_ci | ( | dataType * | V, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | rowVStride, | ||
| int32_t * | sortIndex, | ||
| dataType * | vBuff, | ||
| uint8_t * | pBlock | ||
| ) |
This function uses the max index values calculated from DSPLIB_singularSort_index_ci to shuffle the rows of U' and V' matrix (i.e. colums of U and V matrix).
Definition at line 164 of file DSPLIB_svd_singular_sorting_ci.cpp.
| void DSPLIB_bidiag_uCol_ci | ( | dataType * | U, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colUStride, | ||
| dataType | half_norm_squared, | ||
| dataType * | U1, | ||
| dataType | scale, | ||
| uint8_t * | pBlock | ||
| ) |
This function implements the Household processing on columns of input U matrix corresponding to the natural implementation.
Definition at line 442 of file DSPLIB_svd_bidiag_uMat_ci.cpp.
| void DSPLIB_bidiag_uRow_ci | ( | dataType * | U, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colUStride, | ||
| dataType * | superdiag, | ||
| dataType * | U1, | ||
| dataType | scale, | ||
| uint8_t * | pBlock | ||
| ) |
This function implements the Household processing on rows of input U matrix corresponding to the natural implementation.
Definition at line 1293 of file DSPLIB_svd_bidiag_uMat_ci.cpp.
| void DSPLIB_bidiag_uFinal_ci | ( | dataType * | U, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colUStride, | ||
| dataType | s, | ||
| dataType * | U1, | ||
| uint8_t * | pBlock | ||
| ) |
This function implements the process corresponding to the "update U" loop in natural implementation.
Definition at line 395 of file DSPLIB_svd_bidiag_uFinal_ci.cpp.
| void DSPLIB_bidiag_v_ci | ( | dataType * | V, |
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colVStride, | ||
| dataType | s, | ||
| dataType * | U1, | ||
| dataType * | U, | ||
| int32_t | colUStride, | ||
| uint8_t * | pBlock | ||
| ) |
This function implements the process corresponding to the "update V" loop in natural implementation.
Definition at line 100 of file DSPLIB_svd_bidiag_vMat_ci.cpp.
| void DSPLIB_diag_negate_v_ci | ( | dataType * | V, |
| int32_t | Ncols, | ||
| int32_t | colVStride, | ||
| uint8_t * | pBlock | ||
| ) |
Negates the values of a row in V.
Definition at line 287 of file DSPLIB_svd_diag_ci.cpp.
| void DSPLIB_diag_epsilon_ci | ( | dataType * | diag, |
| dataType * | superdiag, | ||
| dataType * | epsilon, | ||
| int32_t | Ncols, | ||
| uint8_t * | pBlock | ||
| ) |
Updates "epsilon" value based on absolute max values from "diag" and "superdiag" vectors.
Definition at line 98 of file DSPLIB_svd_diag_ci.cpp.
| void DSPLIB_diag_rotation_check_ci | ( | dataType * | diag, |
| dataType * | superdiag, | ||
| dataType | epsilon, | ||
| int32_t * | m, | ||
| int32_t * | rotation_test, | ||
| int32_t | Ncols, | ||
| uint8_t * | pBlock | ||
| ) |
Updates values of "m" and "rotation_test" flag vased on the values present in "diag", "superdiag" and "epsilon".
Definition at line 170 of file DSPLIB_svd_diag_ci.cpp.
| void DSPLIB_diag_rotation_proc_ci | ( | dataType * | U, |
| int32_t | startRow, | ||
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | rowUStride, | ||
| dataType * | cU, | ||
| dataType * | sU, | ||
| uint8_t * | pBlock | ||
| ) |
Updates rows of U' based on the precalculated cU and sU vectors.
Definition at line 845 of file DSPLIB_svd_diag_ci.cpp.
| void DSPLIB_singularSort_index_ci | ( | dataType * | singular_values, |
| dataType * | singularBuffer, | ||
| int32_t * | maxIndArr, | ||
| int32_t | Ncols, | ||
| uint8_t * | pBlock | ||
| ) |
This function sorts the singular values in descending order and also records the max index values for shuffling of U and V matrix columns.
Definition at line 89 of file DSPLIB_svd_singular_sorting_ci.cpp.
| void DSPLIB_diag_sqrt_ci | ( | dataType * | superdiag, |
| dataType * | diag, | ||
| int32_t | length, | ||
| uint8_t * | pBlock | ||
| ) |
Calculates the reciprocal of square-roots of "diag" and "superdiag" vectors.
Definition at line 339 of file DSPLIB_svd_diag_ci.cpp.
| void DSPLIB_svd_blk_move_ci | ( | dataType * | pOut, |
| dataType * | pIn, | ||
| int32_t | Nrows, | ||
| int32_t | Ncols, | ||
| int32_t | colOutStride, | ||
| int32_t | colInStride, | ||
| uint8_t * | pBlock | ||
| ) |
Copy input matrix pIn to pOut.
Definition at line 155 of file DSPLIB_svd_common_ci.cpp.
| void DSPLIB_bidiag_uFinal_init_ci | ( | DSPLIB_kernelHandle | handle | ) |
Definition at line 40 of file DSPLIB_svd_bidiag_uFinal_ci.cpp.
| void DSPLIB_diag_proc_init_ci | ( | DSPLIB_kernelHandle | handle | ) |
Definition at line 36 of file DSPLIB_svd_diag_ci.cpp.
| void DSPLIB_singularSort_swap_init_ci | ( | DSPLIB_kernelHandle | handle | ) |
Definition at line 40 of file DSPLIB_svd_singular_sorting_ci.cpp.
| void DSPLIB_bidiag_u_init_ci | ( | DSPLIB_kernelHandle | handle | ) |
Definition at line 41 of file DSPLIB_svd_bidiag_uMat_ci.cpp.
| void DSPLIB_bidiag_v_init_ci | ( | DSPLIB_kernelHandle | handle | ) |
Definition at line 39 of file DSPLIB_svd_bidiag_vMat_ci.cpp.
| void DSPLIB_svd_matTrans_init_ci | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_svdInitArgs * | kerInitArgs | ||
| ) |
Definition at line 39 of file DSPLIB_svd_common_ci.cpp.
|
inline |
Definition at line 443 of file DSPLIB_svd_priv.h.
| template float getRecip | ( | float | value | ) |
| template double getRecip | ( | double | value | ) |