![]() |
DSPLIB User Guide
|
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_qrd_solver.
Definition in file DSPLIB_qrd_solver_priv.h.
Go to the source code of this file.
Data Structures | |
| struct | DSPLIB_qrd_solver_PrivArgs |
| Structure that is reserved for internal use by the kernel. More... | |
Macros | |
| #define | DSPLIB_QRD_SOLVER_IXX_IXX_OXX_PBLOCK_SIZE (9 * SE_PARAM_SIZE) |
| Macro to define the size of bufPblock array of DSPLIB_qrd_solver_PrivArgs structure. More... | |
Typedefs | |
| typedef DSPLIB_STATUS(* | pFxnDSPLIB_qrd_solver_exec) (DSPLIB_kernelHandle handle, void *restrict pQ, void *restrict pR, void *restrict pB, void *restrict pY, void *restrict pX, void *restrict pD, void *restrict pR1) |
| This is a function pointer type that conforms to the declaration of DSPLIB_qrd_solver_exec_ci and DSPLIB_qrd_solver_exec_cn. More... | |
Functions | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_qrd_solver_init_ci (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams1D_t *bufParamsB, DSPLIB_bufParams1D_t *bufParamsY, DSPLIB_bufParams1D_t *bufParamsX, const DSPLIB_qrdSolverInitArgs *pKerInitArgs) |
| This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_solver_init. More... | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_qrd_solver_exec_ci (DSPLIB_kernelHandle handle, void *restrict pQ, void *restrict pR, void *restrict pB, void *restrict pY, void *restrict pX, void *restrict pD, void *restrict pR1) |
| This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_solver_exec. More... | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_qrd_solver_init_cn (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams1D_t *bufParamsB, DSPLIB_bufParams1D_t *bufParamsY, DSPLIB_bufParams1D_t *bufParamsX, const DSPLIB_qrdSolverInitArgs *pKerInitArgs) |
| This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_solver_init. More... | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_qrd_solver_exec_cn (DSPLIB_kernelHandle handle, void *restrict pQ, void *restrict pR, void *restrict pB, void *restrict pY, void *restrict pX, void *restrict pD, void *restrict pR1) |
| This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_solver_exec. More... | |
| #define DSPLIB_QRD_SOLVER_IXX_IXX_OXX_PBLOCK_SIZE (9 * SE_PARAM_SIZE) |
Macro to define the size of bufPblock array of DSPLIB_qrd_solver_PrivArgs structure.
Definition at line 39 of file DSPLIB_qrd_solver_priv.h.
| typedef DSPLIB_STATUS(* pFxnDSPLIB_qrd_solver_exec) (DSPLIB_kernelHandle handle, void *restrict pQ, void *restrict pR, void *restrict pB, void *restrict pY, void *restrict pX, void *restrict pD, void *restrict pR1) |
This is a function pointer type that conforms to the declaration of DSPLIB_qrd_solver_exec_ci and DSPLIB_qrd_solver_exec_cn.
Definition at line 46 of file DSPLIB_qrd_solver_priv.h.
| DSPLIB_STATUS DSPLIB_qrd_solver_init_ci | ( | DSPLIB_kernelHandle | handle, |
| DSPLIB_bufParams2D_t * | bufParamsQ, | ||
| DSPLIB_bufParams2D_t * | bufParamsR, | ||
| DSPLIB_bufParams1D_t * | bufParamsB, | ||
| DSPLIB_bufParams1D_t * | bufParamsY, | ||
| DSPLIB_bufParams1D_t * | bufParamsX, | ||
| const DSPLIB_qrdSolverInitArgs * | pKerInitArgs | ||
| ) |
This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_solver_init.
This function determines the configuration for the streaming engine resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_qrd_solver_exec_ci would be called later independently by the application. When DSPLIB_qrd_solver_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_qrd_solver_exec_ci does not lose cycles to determine the hardware configuration.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsQ | : Pointer to the structure containing dimensional information of Q matrix |
| [in] | bufParamsR | : Pointer to the structure containing dimensional information of R matrix |
| [in] | bufParamsB | : Pointer to the structure containing dimensional information of input vector B |
| [in] | bufParamsY | : Pointer to the structure containing dimensional information of temporary vector Y |
| [out] | bufParamsX | : Pointer to the structure containing dimensional information of ouput vector X |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 604 of file DSPLIB_qrd_solver_ci.cpp.
| DSPLIB_STATUS DSPLIB_qrd_solver_exec_ci | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pQ, | ||
| void *restrict | pR, | ||
| void *restrict | pB, | ||
| void *restrict | pY, | ||
| void *restrict | pX, | ||
| void *restrict | pD, | ||
| void *restrict | pR1 | ||
| ) |
This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_solver_exec.
The function implements optimized version for DSPLIB_qrd_solver_exec.
| [in] | handle | : Active handle to the kernel. |
| [in] | pQ | : Pointer to the input matrix Q. |
| [in] | pR | : Pointer to the input matrix R. |
| [in] | pB | : Pointer to the input vector B. |
| [in] | pY | : Pointer to the temporary vector Y. |
| [out] | pX | : Pointer to the output vector X. |
| [in] | pD | : Pointer to the Scratch buffer D. |
| [in] | pR1 | : Pointer to the Scratch buffer for transposed matrix of R. |
Definition at line 652 of file DSPLIB_qrd_solver_ci.cpp.
| DSPLIB_STATUS DSPLIB_qrd_solver_init_cn | ( | DSPLIB_kernelHandle | handle, |
| DSPLIB_bufParams2D_t * | bufParamsQ, | ||
| DSPLIB_bufParams2D_t * | bufParamsR, | ||
| DSPLIB_bufParams1D_t * | bufParamsB, | ||
| DSPLIB_bufParams1D_t * | bufParamsY, | ||
| DSPLIB_bufParams1D_t * | bufParamsX, | ||
| const DSPLIB_qrdSolverInitArgs * | pKerInitArgs | ||
| ) |
This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_solver_init.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsQ | : Pointer to the structure containing dimensional information of Q matrix |
| [in] | bufParamsR | : Pointer to the structure containing dimensional information of R matrix |
| [in] | bufParamsB | : Pointer to the structure containing dimensional information of input vector B |
| [in] | bufParamsY | : Pointer to the structure containing dimensional information of temporary vector Y |
| [out] | bufParamsX | : Pointer to the structure containing dimensional information of ouput vector X |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 31 of file DSPLIB_qrd_solver_cn.cpp.
| DSPLIB_STATUS DSPLIB_qrd_solver_exec_cn | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pQ, | ||
| void *restrict | pR, | ||
| void *restrict | pB, | ||
| void *restrict | pY, | ||
| void *restrict | pX, | ||
| void *restrict | pD, | ||
| void *restrict | pR1 | ||
| ) |
This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_solver_exec.
| [in] | handle | : Active handle to the kernel. |
| [in] | pQ | : Pointer to the input matrix Q. |
| [in] | pR | : Pointer to the input matrix R. |
| [in] | pB | : Pointer to the input vector B. |
| [in] | pY | : Pointer to the temporary vector Y. |
| [out] | pX | : Pointer to the output vector X. |
| [in] | pD | : Pointer to the Scratch buffer D. |
| [in] | pR1 | : Pointer to the Scratch buffer for transposed matrix of R. |
Definition at line 60 of file DSPLIB_qrd_solver_cn.cpp.